Hi,
I want to run LittleFS on an external QSPI NOR flash chip from MXIC (MX25R4035F). I found that they published a PACK file to import into e2studio at the below URL. I'm also attaching the ZIP file to this message.
I followed all the steps - copy the .pack file into my "Renesas\e2_studio\internal\projectgen\ra\packs\" folder, import it using File -> Import -> CMSIS Pack. I even created a brand new project so that I'm sure my project's older FSP version does not affect their pack, which was created for FSP 4.e2studio goes through the process and tells me that the pack was imported correctly (attached), but then when I want to add their driver to LittleFS it does not give me the option as mentioned in their document "Application Note for LittleFS MXIC Middleware_v2.0.pdf" (see screenshot "pack import screenshot - ideal.png").
So how can I get e2studio to display the imported pack file?
PS:I see there are "packs" folders in 2 places:c:\Renesas\e2_studio\internal\projectgen\ra\packs\c:\Users\Johann.Kok\.eclipse\com.renesas.platform_1435879475\internal\projectgen\ra\packs\
The above-mentioned pack file is in both locations, but should I delete one of the locations? My e2studio is located in the folder "C:\Renesas\e2_studio\eclipse"?
regardsJohann
https://www.mxic.com.tw/Lists/MoreSoftware/Attachments/225/renesas-fsp-v4.0.0_QSPI-OSPI-littlefs-mxic-middleware.zip
What I get:
What I should see:
Looks like there is an error with the pack files from Macronix (the file toolingSupport.xml in the pack files doesn't reference the XML file in the .module_descriptions folder in the pack files)
The…