Interrupt handler in C - a couple of questions

When writing interrupt handlers, it is obviously necessary to clear bit 16 of IESLR[] to prevent the handler routine running over and over again,  but is there an easy way of knowing which IESLR register needs its 16th bit cleared?


In the configuration tab for setting up interrupts, does the automatically generated code take care of setting the relevant bits ins ISER[0] to enable the interrupts?

Top Replies

  • in reply to Ian +1 verified
    Where are these functions documented? I have done a text search of the FSP manual and drawn a blank.

    When you generate code , search in 'ra' folder, in your project in e2studio

  • In the configuration tab for setting up interrupts, does the automatically generated code take care of setting the relevant bits ins ISER[0] to enable the interrupts?

    mostly yes, but it depends in the complex hardware . Like in timer in PTP , there are driver functions which lets you enable IRQ on rising or falling edge.  You can also check OPEN or ENABLE driver calls to verify this. On serial port drivers interrupts are configured by drivers. You can however select priority and callback function in GUI.

    When writing interrupt handlers, it is obviously necessary to clear bit 16 of IESLR[] to prevent the handler routine running over and over again,  but is there an easy way of knowing which IESLR register needs its 16th bit cleared?

    When you configure interrupt in IDE it also shows ISR names, if you look for the code , you will find out that flags are cleared at the end using 

    R_BSP_IrqStatusClear(irq);
     also you can get the answer of your first question there. 

    I think this is how you can see which interrupt has occurred.

    IRQn_Type             irq             = R_FSP_CurrentIrqGet();


  • Where are these functions documented? I have done a text search of the FSP manual and drawn a blank.

  • Where are these functions documented? I have done a text search of the FSP manual and drawn a blank.

    When you generate code , search in 'ra' folder, in your project in e2studio