Hello
I'm trying to build our project that uses a Bootloader. The project is linked to the bootloader as described and in e2studio IDE everything works fine - but not trying to build headless (in CI).
diff --git a/.cproject b/.cproject index 785139065391..166350b54b6a 100644 --- a/.cproject +++ b/.cproject @@ -3,6 +3,9 @@ <storageModule moduleId="org.eclipse.cdt.core.settings"> <cconfiguration id="com.renesas.cdt.managedbuild.gnuarm.config.elf.release.826160552"> <storageModule buildSystemId="org.eclipse.cdt.managedbuilder.core.configurationDataProvider" id="com.renesas.cdt.managedbuild.gnuarm.config.elf.release.826160552" moduleId="org.eclipse.cdt.core.settings" name="Release"> + <macros> + <stringMacro name="BootloaderDataFile" type="VALUE_PATH_FILE" value="${workspace_loc:ConvectorControlBootloader}/Release/ConvectorControlBootloader.bld"/> + </macros> <externalSettings/> <extensions> <extension id="org.eclipse.cdt.core.ELF" point="org.eclipse.cdt.core.BinaryParser"/>
I invoke the headless builder with the following command
e2studio -verbose -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data <path_to_workspace> -import <path_to_bootloader_in_workspace> -import <path_to_application_in_workspace> -cleanBuild allIt successfully builds first the bootloader and then the application, both get built. But then it fails at the last step:
e2studio -verbose -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data <path_to_workspace> -import <path_to_bootloader_in_workspace> -import <path_to_application_in_workspace> -cleanBuild all
Invoking 'DDSC Bundle Builder' on '/ConvectorControl'.
There is also a popup window that says "An error has occured See the log file". I attached that logfile and the log from my console.
Any help would be appreciated. I cannot figure out what is missing and there is very little to no error-messages that I can understand.Console Log: https://pastebin.com/UEcze4zSLogfile from e2studio (in .metadata/.log): https://pastebin.com/HEmqzHBjI'm working with Ubuntu 22.04, e2studio 2023.01 and FSP 4.2.0
Hello!Thanks for forwarding this issue to the dev-team. I tried again with FSP 4.4.0 and e2studio 2023.04 and my CI pipeline magically worked.Thanks for fixing!
Thank you for your report - this has now been reported to the e2 studio development team for investigation