Cannot adding Software Components via Smart Configurator in e2Studio

Hi all,

I have a problem in e2Studio.

Since I have installed the e2Stidio Version 2023-01 (23.1.0) I am not able to add Software Components via Smart Configurator. It is independent if I select a RX- oder RZ-Type.

I have this e2Studio-version also installed on my PC in the company and there it works without problems. On my PC at home I have the problems as described above. Follwing two screenshots what happend. Has anyone an idea, whats wrong?

Thanks

Elektroniker

Edit: Is solved. I have installed the components I need manually.