Updated to e2 Studio 2023-10 - Debug history missing

Hello everyone,

today I updated my installation (e2 Studio 2022-10) to e2 Studio 2023-10, SSP 2.5.0. So far the µC program works the same, but I am missing the 'old' Debug History. In the old version of e2 Studio there were three easy to reach buttons on the far left and a combobox with possible launch configurations to choose from (blacked out for privacy).

In the new e2 Studio however, this is missing and I can't for the life of me figure out how to get it back. I tried customizing the perspectives and views, but I can't seem to find it. Can anybody help me with this? The new view:

Thanks a lot

Christoph

Parents
  • Hi Christoph,

    Yes the UI was streamlined in 2023-07 and 2023-10.

    Many users were not fond of the Launch Bar UI from our feedback. We listened and removed it from the default use case.

    You can however re-enable it here in the Window->Preferences menu item:

    Hope it works well for your usage case.

    Thanks,

    Mark.

  • Hi Mark,

    Thank you very much for your answer. I can of course only speak for myself, but I was really missing the launch bar, especially being able to see at a glance which project will be run when I click the Debug button - much easier with the Combo Box.

    Kind Regards,

    Christoph

Reply Children
No Data