E2Studio Add/Update Tool chain after FSP update

Dear All,

<Context>

- We have created our project starting from fsp 4.6.0 and the associated e2studio. The project were using the following Tool chain: GCC ARM embedded 12.2.1.202302.

Now we want to move to the latest FSP 5.1.0 which has as a Tool Chain LLVM Embeded Tool.

- While importing our project, as in FSP 5.1.0, GCC ARM embedded 12.2.1.202302 is not available, we wanted to add in Renesas Toolchain Management to add it but we got the following errors:

Environment: Linux

<Question>

Do we miss some steps which leads to have the download of the tool chain failing?

In advance thanks for any feedback,