cannot open linker script file fsp.ld

Hello,

I have used e2stuido (2023/10) on the windows 10 OS.

When I created new project this problem always has been showed on the IDE:

The IDE  cannot open linker script file fsp.ld:

c:/program files (x86)/gnu arm embedded toolchain/12.2 mpacbti-rel1/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: cannot open linker script file fsp.ld: No such file or directory

collect2.exe: error: ld returned 1 exit status

make: *** [makefile:97: demo.elf] Error 1

Many times tried and updated toolchain from the toolchain editor but the problem has insisted.

E2studio: 2023\10

Windows OS: Windows 10

MCU: Renesas RA series (RA2L1)

Could you please help me to solve this problem?

Parents Reply Children
No Data