e-AI translator license file expired.

Hello there

e2 studio version:2023.10.

The latest e-AI translator V3.1.0 installed.

According to the UM, copy the license.txt (download from e-AI Translator License Extension  for V3.10  expired end of Jan 24)

to the plugin folder.

When I try to use the translator in the studio,  license check window showing the license is expired, even I select the license file, the error still remains.

BR

Tony