Hi,
I am using SH72531 and E10A USB EMULATOR(HS0005KCU01H). Currently I am using the emulator to run the code.
I want to program the flash i.e run my application code through flash. Is it possible using the E10A USB EMULATOR(HS0005KCU01H) ?
If not what is the procedure to program the flash?
Regards
Ali
E10A-USB is not meant to be used for flash programming. But if you downloaded the code during debugging to your SH72531, you should be able to run it when you disconnect E10A-USB and switch emulator function on the processor off.
You can use FDT and E8a for flash programming on SH72531.