Can the E2 Lite Emulator be installed under HEW?

I recently purchased an E2 Lite emulator, and installed the USB Driver for Renesas MCU Tools V2.77.00 (for 64-bit version of Windows OS) from the E2 Lite website downloads pages. I opened HEW (4.09.01.007) and could not find any indication of how to select the E2 Lite as the debugger.

A little background:

After installation of the USB driver, a program called "E2 Self Check Program" became available. However, with the E2 Lite plugged into the USB port, the program fails to detect the E2 Lite. Is this important that it is not recognized? I have checked that the E2 Lite shows up under Device hardware (running Windows 7 64 bit SP1). Will this impact any chances of having the E2 Lite recognized under HEW?

Has anyone any experience in installing E2 Lite under HEW? If so, would you be able to share on how this is done? For example, is there any other driver or utility that needs to be installed in order for HEW to recognize the E2 Lite, or is HEW not capable of recognizing it?

I have not been able to find any reference to E2 Lite working under HEW, so far.

 

Thanks.

Parents Reply Children
No Data