ID Code for R8C29 with e8a and HEW

I want to get the ID Code for the debugging. 

What I could see is the starup file "Section30"

Could you help me to find the ID Code back? 

Thank you for the help! 

Here is the code for Section30

for R8C/Tiny

;===============================================================
; fixed vector section
;---------------------------------------------------------------
.section fvector,ROMDATA ; fixed vector table
.org 0ffdcH

.glb _IrqLowVoltage

;UDI:
; .lword dummy_int
;OVER_FLOW:
; .lword dummy_int
;BRKI:
; .lword dummy_int
;ADDRESS_MATCH:
; .lword dummy_int
;SINGLE_STEP:
; .lword dummy_int
;WDT: Interrupt bei Unterspannung
.org 0fff0H
.lword _IrqLowVoltage | 0FF000000h
;RESERVED:
; .lword dummy_int
;RESERVED:
; .lword dummy_int

.org 0fffcH
RESET:
.lword start
;
; ID code check function
; .id "CodeChk"
;
; option function select register
;
.ofsreg 09FH

.endif ; __R8C