Dears,
I'm a newer to Renesas, recently I was assigned to a project which uses the RX62T series mcu as controller, when I finished installing HEW, and trying to create a hello project, I found that I can't the select the emulator I have and installed, only simulators, the emulator and the board RSKRX62T should all be good, as well as the E1 USB driver, as I can use the E1 emulator together with the flash programmer to read and program the board.
Did I miss any plug-in to the HEW? I looked for long time but found nothing.
Any comments are appreciated!
Hello Seven!
I found a post in Renesas KnowlegeBase that is related to your inquiry. Kindly refer to this url: How to connect to E1/E20 Emulator with RX High-Performance Embedded Workshop | Renesas Customer…
I found a post in Renesas KnowlegeBase that is related to your inquiry. Kindly refer to this url: How to connect to E1/E20 Emulator with RX High-Performance Embedded Workshop | Renesas Customer Hub
I hope that will be helpful. All the best!
SaiRenesasRulz Forum Moderator
https://renesasrulz.com/https://academy.renesas.com/ en-support.renesas.com/knowledgeBase
Hi Seven, Have you checked Sai's response? Did it answer your question?
HeraldRenesasRulz Forum Moderatorhttps://renesasrulz.com/https://academy.renesas.com/en-us.knowledgebase.renesas.com/
Dear Sai,
Many thanks for your help, I didn't install the debugger, also didn't know that I need to register it in the HEW, now problem is solved!
Yes, it does, you can close the thread now