CS+ for CC can't find uint sizes

Hello,
i have a problem with the CS+ for CC IDE.
I wanted to run some sample code by initializing a variable like uint8_t test = 5.
Sadly, the IDE says that it can't find this datatype, even after the include of stddef.h.
My error message reads:
E0520020: Identifier "uint8_t" is undefined
I hope someone can explain to me where my error is.
Thanks

Parents
  • Would you mind telling us which compiler version you use? Have you checked stdint.h includes the definition you are looking for? Have you checked that the compiler can open the include file (e.g. by inserting an invalid statement in it or by checking the list file of your C source)?

Reply
  • Would you mind telling us which compiler version you use? Have you checked stdint.h includes the definition you are looking for? Have you checked that the compiler can open the include file (e.g. by inserting an invalid statement in it or by checking the list file of your C source)?

Children
No Data