You are currently reviewing an older revision of this page.
[1]Click on the title to open the thread.
[2]When you open Thread, there is a "Reply" indication on the bottom left of every Post, and the entry frame is displayed when clicked.
(*) If you not a Member of a Group, "Reply"Button and the entry box will not be displayed.
(*)When you want to switch to the editor with functions such as character qualification, please click "Use rich formatting" in the lower right.
If you press "Quote" above the "Description" box, the post sentence displayed above it will be quoted.
After filling in, when you click "Post", the created Reply will be posted.
(Note) Regardless of which post in the thread you create Reply, the most recent Reply will be displayed at the bottom of the thread.
Reply to a Reply
In addition to Reply to a Post, you can also Reply to a Reply.
In case of Reply to a Reply, comment "In reply to ..." is added at the beginning of the comment.