Setting the time from the collector application when the Current Time Service is enabled does not work.

Setting the time from the collector application when the Current Time Service is enabled does not work. The Current Time characteristic value is set to writable and the collector recognizes the fact that the characteristic is writable. The collector follows the Current Time Service specification 1.1 for setting the time and when it sees that it is writable, the collector attempts to write the current time. The RL78 responds with 'out of resources'. This bug needs to be fixed.

Parents
  • I confirmed "API Reference Manual: TIP of Bluetooth® Low Energy Protocol Stack(R01UW0106)".
    To Appendix B Referenced Documents, "26. Current Time Service Specification v1.0, Bluetooth SIG" is mentioned.
    I think that Support profile is Current Time Service Specification v1.0.
Reply
  • I confirmed "API Reference Manual: TIP of Bluetooth® Low Energy Protocol Stack(R01UW0106)".
    To Appendix B Referenced Documents, "26. Current Time Service Specification v1.0, Bluetooth SIG" is mentioned.
    I think that Support profile is Current Time Service Specification v1.0.
Children
No Data