Hello Support Team,
Where can I find a copy (ZIP file) of source code for Dialog Serial Port Service version 3.150.2, which includes SDK version 3.0.6.0?
The DA14580-based product I support uses a modified version of said source code, but I need to know what the unmodified source code looked like.
I have searched your company's web site without success. Please help! Thanks!
Hi b.la_garrett,
DSPS version 3.150.2 is not available on our support site, as it is based on SDK3 which a very old version of SDK and it is not currently supported. From the DSPS portal, you are able to download the latest version of DSPS which is based on SDK5.0.4. Please take a look:
https://www.dialog-semiconductor.com/products/dialog-serial-port-service-dsps
However, I will ask internally if it possible to share DSPS version 3.150.2.
If you are starting a new design or project, we recommend to start with our newest Smartbond device named DA14531. The SDK is much improved, we have a lot of code examples and improved documentation, and there is also software roadmap support. There is not any software roadmap support for DA14580 product family and SDK5.
Please take a look at our new BLE device:
https://www.dialog-semiconductor.com/products/connectivity/bluetooth-low-energy/products/da14531
Thanks, PM_DIalog
Support Team,
Thanks for responding promptly. Yes, please inquire about sharing DSPS 3.150.2 + SDK 3.0.6.0 with me.
This is very important because I need to migrate the product from 3.150.2 to 5.150.2, but Dialog Semiconductor has dramatically changed the DSPS and SDK source code between those two versions. Folder names and file names have changed. File contents have changed. I cannot simply use a "diff" tool to compare our customized 3.150.2 to 5.150.2 and then migrate our modifications to 5.150.2. Instead, I will need to "diff" the original 3.150.2 to our modified version so I understand exactly what was modified, and then somehow migrate each change to where it seems to best fit within 5.150.2.
I do not know how to migrate our product from 3.150.2 to 5.150.2 unless I can get the original DSPS 3.150.2 + SDK 3.0.6.0 source code base and perform a "diff".
Thanks very much for your help!
Hi b.la_garrett,,
I will send you an email in your registered email address.
Thanks, PM_Dialog
Thank you very much. I now have everything I need.
Please send me DA16200 DA16600 FreeRTOS SDK Image v3.2.2.0 source code. I cannot upgrade to v3.2.6.0 without having the pristine v3.2.2.0 code so I can compare changes we made to it.
Hi Burt,This ticket here is quite old and the SDK v3 does not refer on the SDK you are looking for DA16200.I have reached out directly into your e-mail with the SDK v3.2.2 for DA16200.Kind Regards,OV_Renesas