current consumption due to SPI FLASH on DA14531 module

I see extended sleep current consumption near 1,2uA on USB basic development  kit, but only when disconnect FLASH after boot (by DIP's). When the flash is still connected, the current is near 24uA. How it looks on DA14531 module? I saw in some docummentation, that SPI FLASH is disconnected after boot. So is it hardware or software disconnected in module? 

The basic question is what extended sleep current is on DA14531 module? 1,2uA (like on dev kit with DIP1-5 OFF) or 24uA (like on dev kit with DIP1-5 ON)?

Parents Reply Children