Hello there!
I am trying to add the SUOTA service in my ibeacon modified firmware.
i have included all SUOTA configuration as per prox reporter and tutorial with changing to undirected advertising by a flag condition. I have #define CFG_PRF_SUOTAR in user_profile_config.h
and it goes in platform_reset_func() while debugging. and if i see the uart logs it stops printing after rwip_schedule(); line no 399 in arch_main.c
log___1 and log___2 are visible.
__STATIC_INLINE void schedule_while_ble_on(void) { printf_string(UART2,"log__1\n"); // BLE clock is enabled while (ble_is_powered()) { //execute messages and events printf_string(UART2,"log___2\n"); rwip_schedule(); printf_string(UART2,"log__3\n"); #if defined (__DA14531__)
And if i comment the #define CFG_PRF_SUOTAR in user_profile_config.h the whole program runs very well without going to reset error.
please guide me about this, How can i add SUOTA service in my code and why this error happening.
https://drive.google.com/file/d/1AiaN8MGnNahLk2umUdgUE7U0qiberwnN/view
please check this zip file.
By defining #define DB_HEAP_SZ 2048 (not 1024) it started to work well.