Hardware:
Custom board using DA14683
SDK:
1.0.14.1081 (last updated in 2018, despite what the new renesas download link says)
Situation:
The DA14683 won't go into extended sleep mode.
I issue the "pm_set_sleep_mode(pm_mode_extended_sleep);" command but the sleep state does not change. The power consumption does not change. From what I can tell it never changes the sleep state.
Questions:
1) How should I go about troubleshooting what is keeping the sleep mode from running? How can I determine what is keeping the code from going into sleep mode?
2) Can you debug the sleep mode operation?
Hi Nathan,
When issuing pm_set_sleep_mode(pm_mode_extended_sleep) the device should go into sleep mode between advertising or connection intervals.
If you could share more information about your firmware it would be very helpful to understand why you are getting increased power consumption. Which SDK project are you using?
Best regards,
PM_Renesas