Hello, what is the difference between the DA14531 and DA14531MOD? In the past, I wrote code for DA14531, can the same code be used for the DA14531MOD?
Thank you
Hi Kerby,Thank you for posting your question online. Yes, your code on DA14531 is going to work on DA14531MOD. The DA14531 SmartBond TINY Module is the first Dialog Semiconductor Bluetooth® Low Energy module…
Hi Kerby,Thank you for posting your question online. Yes, your code on DA14531 is going to work on DA14531MOD. The DA14531 SmartBond TINY Module is the first Dialog Semiconductor Bluetooth® Low Energy module based on world’s lowest power DA14531 SoC. The module offers a unique combination of the lowest power and the integration of all external components including antenna at a very affordable price. Also, the DA14531MOD has an integrated SPI Flash while DA14531 will need one externally. You might need to change inside the user_periph_setup.h (on your old code) your GPIOs configuration if you want to use the SPI Flash on DA14531MOD.Kind Regards,OV_Renesas