DA14531MOD SPI flash configuration

Hello,

I have been facing problems while erasing , writing and reading data from flash memory on the DA14531MOD.

The problem might be in the configurations made by me in the following fuction.

static const spi_flash_cfg_t spi_flash_cfg = {
.dev_index = (uint8_t)P25Q11U_MAN_DEV_ID,
.jedec_id = P25Q11U_JEDEC_ID,
.chip_size = SPI_FLASH_DEV_SIZE,
};

by running the example code i could identify the flash chip to be P25Q11U.

The dev_indix for P25Q11U couldn't be found in spi_flash.h.

what can be the better way of configuring the spi flash?

Thank you.

  • Hi Sumo,

    Thank you for posting your question online.
    I understand your issue and I was able to replicate it.
    I worked on the empty_peripheral_template example and I followed the DA14531 SDK6 Peripheral Drivers Tutorial:5. DA14531 SPI Flash — DA145XX Tutorial SDK peripherals (renesas.com)
    On the user_periph_setup.h file I set the SPI pins as shown below:

    /****************************************************************************************/
    /* SPI configuration                                                                    */
    /****************************************************************************************/
    // Define SPI Pads
    #if defined (__DA14531__)
        #define SPI_EN_PORT             GPIO_PORT_0
        #define SPI_EN_PIN              GPIO_PIN_1
    
        #define SPI_CLK_PORT            GPIO_PORT_0
        #define SPI_CLK_PIN             GPIO_PIN_4
    
        #define SPI_DO_PORT             GPIO_PORT_0
        #define SPI_DO_PIN              GPIO_PIN_0
    
        #define SPI_DI_PORT             GPIO_PORT_0
        #define SPI_DI_PIN              GPIO_PIN_3
    
    #elif !defined (__DA14586__)
        #define SPI_EN_PORT             GPIO_PORT_0
        #define SPI_EN_PIN              GPIO_PIN_3
    
        #define SPI_CLK_PORT            GPIO_PORT_0
        #define SPI_CLK_PIN             GPIO_PIN_0
    
        #define SPI_DO_PORT             GPIO_PORT_0
        #define SPI_DO_PIN              GPIO_PIN_6
    
        #define SPI_DI_PORT             GPIO_PORT_0
        #define SPI_DI_PIN              GPIO_PIN_5
    #endif

    And on user_periph_setup.c file:
    void GPIO_reservations(void)
    {
    /*
        i.e. to reserve P0_1 as Generic Purpose I/O:
        RESERVE_GPIO(DESCRIPTIVE_NAME, GPIO_PORT_0, GPIO_PIN_1, PID_GPIO);
    */
    
    #if defined (CFG_PRINTF_UART2)
        RESERVE_GPIO(UART2_TX, UART2_TX_PORT, UART2_TX_PIN, PID_UART2_TX);
    #endif
    
    #if !defined (__DA14586__)
     //   RESERVE_GPIO(SPI_EN, SPI_EN_PORT, SPI_EN_PIN, PID_SPI_EN);
    #endif
    		RESERVE_GPIO(SPI_FLASH_CS, SPI_EN_PORT, SPI_EN_PIN, PID_SPI_EN);
    		RESERVE_GPIO(SPI_FLASH_CLK, SPI_CLK_PORT, SPI_CLK_PIN, PID_SPI_CLK);
    		RESERVE_GPIO(SPI_FLASH_DO, SPI_DO_PORT, SPI_DO_PIN, PID_SPI_DO);
    		RESERVE_GPIO(SPI_FLASH_DI, SPI_DI_PORT, SPI_DI_PIN, PID_SPI_DI);
    }

    void set_pad_functions(void)
    {
    /*
        i.e. to set P0_1 as Generic purpose Output:
        GPIO_ConfigurePin(GPIO_PORT_0, GPIO_PIN_1, OUTPUT, PID_GPIO, false);
    */
    
    #if defined (__DA14586__)
        // Disallow spontaneous DA14586 SPI Flash wake-up
        GPIO_ConfigurePin(GPIO_PORT_2, GPIO_PIN_3, OUTPUT, PID_GPIO, true);
    #else
        // Disallow spontaneous SPI Flash wake-up
        GPIO_ConfigurePin(SPI_EN_PORT, SPI_EN_PIN, OUTPUT, PID_SPI_EN, true);
    #endif
    
    #if defined (CFG_PRINTF_UART2)
        // Configure UART2 TX Pad
        GPIO_ConfigurePin(UART2_TX_PORT, UART2_TX_PIN, OUTPUT, PID_UART2_TX, false);
    #endif
    	
    		GPIO_ConfigurePin(SPI_EN_PORT, SPI_EN_PIN, OUTPUT, PID_SPI_EN, true);
    		GPIO_ConfigurePin(SPI_CLK_PORT, SPI_CLK_PIN, OUTPUT, PID_SPI_CLK, false);
    		GPIO_ConfigurePin(SPI_DO_PORT, SPI_DO_PIN, OUTPUT, PID_SPI_DO, false);
    		GPIO_ConfigurePin(SPI_DI_PORT, SPI_DI_PIN, INPUT, PID_SPI_DI, false);
    
    }

    void periph_init(void)
    {
    #if defined (__DA14531__)
        // In Boost mode enable the DCDC converter to supply VBAT_HIGH for the used GPIOs
        syscntl_dcdc_turn_on_in_boost(SYSCNTL_DCDC_LEVEL_3V0);
    #else
        // Power up peripherals' power domain
        SetBits16(PMU_CTRL_REG, PERIPH_SLEEP, 0);
        while (!(GetWord16(SYS_STAT_REG) & PER_IS_UP));
        SetBits16(CLK_16M_REG, XTAL16_BIAS_SH_ENABLE, 1);
    #endif
    
        // ROM patch
        patch_func();
    
        // Initialize peripherals
    #if defined (CFG_PRINTF_UART2)
        // Initialize UART2
        uart_initialize(UART2, &uart_cfg);
    #endif
    
        spi_cfg_t spi_flash_cfg = { .spi_ms = SPI_MS_MODE_MASTER,
                                    .spi_cp = SPI_CP_MODE_0,
                                    .spi_speed = SPI_SPEED_MODE_4MHz,
                                    .spi_wsz = SPI_MODE_8BIT,
                                    .spi_cs = SPI_CS_0,
                                    .cs_pad.port = SPI_EN_PORT,
                                    .cs_pad.pin = SPI_EN_PIN,		
                            #if defined (__DA14531__)
                                    .spi_capture = SPI_MASTER_EDGE_CAPTURE
                            #endif
                                    };
    
        spi_initialize(&spi_flash_cfg);
        // Set pad functionality
        set_pad_functions();
    
        // Enable the pads
        GPIO_set_pad_latch_en(true);
    }

    On user_empty_peripheral_template.c file:
    void user_on_init(void)
    {
        arch_printf("\n\r%s", __FUNCTION__);
    
        default_app_on_init();
    
        // Disable HW RST on P0_0 so it can be used as SPI MOSI.
        GPIO_Disable_HW_Reset();
    
        int8_t ret;
        ret = spi_flash_block_erase(0x20000, SPI_FLASH_OP_SE);
        arch_printf("\n\rErase Status: %d", ret);
    
        uint16_t bytes_written;
        uint8_t data[16] = { 0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 1, 2, 3, 4, 5 };
    
        ret = spi_flash_write_data(&data[0], 0x20000, sizeof(data), &bytes_written);
        arch_printf("\n\rWrite Status: %d", ret);
        arch_printf("\n\rBytes Written: %d", bytes_written);
    
        uint16_t bytes_read;
        uint8_t data_read[16] = { 0 };
    
        ret = spi_flash_read_data(&data_read[0], 0x20000, sizeof(data_read), &bytes_read);
        arch_printf("\n\rRead Status: %d", ret);
        arch_printf("\n\rBytes Read:");
        while (bytes_read) {
            arch_printf(" %d", data_read[sizeof(data_read) - bytes_read]);
            bytes_read--;
        }
    
        // Reduce power consumption by putting flash into sleep mode */
        spi_flash_power_down();
    
        // Re-enable HW reset input (must be disabled if/when further operation on
        // external flash are performed) - must set as input first!
        GPIO_ConfigurePin(SPI_DO_PORT, SPI_DO_PIN, INPUT_PULLDOWN, PID_GPIO, false);
        GPIO_Enable_HW_Reset();
    }

    After that I was able to connect to the device via SmartSnippets Toolbox and see the data I had written on the SPI Flash:


    Kind Regards,
    OV_Renesas

  • Hello,

    I could successfully write in the flash memory, at memory location 0x2A000.

    I am getting an error while reading the memory location. 

    where can I get list of readable and writable flash memory locations?

  • Hi Sumo,

    Thank you for the reply.
    Are you working with one of your Development Kits? If yes, which one?
    If you are working with our Development Kit Pro your board configuration should look like this:

    With this configuration you should be able to Write/Read on the SPI Flash of the DA14531MOD (P25Q11U).
    If your configuration looks like this:
     
    With this configuration you are should be able to Write/Read on the SPI Flash integrated on the Development Kit Pro (MX25R2035).
    You stated you successfully wrote in the flash memory, at memory location 0x2A000.
    The memory location 0x2A000 exceeds the size of the SPI Flash on DA14531MOD. 

    The maximum value for the SPI Flash on the DA14531MOD is 0x1F000

    As you can see on the SDK6 Peripheral Drivers Tutorial:5. DA14531 SPI Flash — DA145XX Tutorial SDK peripherals (renesas.com)
    On 5.1 you can find the SPI Flash Memory Layout for the Development Kit:


    Exactly the same SPI Flash Memory Layout applies for the SPI Flash of the DA14531MOD but you do not have the last 128kB available for user data storage.
    If you want to implement SUOTA on your project, you should refer on the SUOTA tutorial here:22. SUOTA Overview — DA145XX Tutorial SDK Getting started (renesas.com)
    For DA14531MOD SPI Flash you should check chapter 27. 


    If you have any further questions, feel free to ask.

    Kind Regards,
    OV_Renesas

  • Thank you!

    So while using the DA14531MOD,

    If I want to store about 30-40 bytes of data in the flash, I will not be able to do that. as the 128kB is not available for user data storage.

    I will have to have an external flash for storing the user application data.

    I misread 1Mb as 1MB, and hence was confused for long period of time.

  • Hi Sumo,

    Thank you for the reply. 
    No, you will not have to use an external flash to store your user application data.
    As you can see on the screenshot I shared on my previous answer, with DA14531MOD SPI Flash you can use:

    You can have up to 74kB for User data storage. The DA14531MOD SPI Flash does not have the last 128kB available.

    Kind Regards,
    OV_Renesas

  • hello,

    I have written successfully @ memory location 0xBD80 and further, but the i am unable to read the same.

    The application stops execution whenever I include spi_flash read command.

  • hello,

    I have written successfully @ memory location 0xBD80 and further, but the i am unable to read the same.

    The application stops execution whenever I include spi_flash read command.

  • Hi Sumo,

    Thank you for the reply.
    Could you please call the following function before trying to read the contents of the Flash: spi_flash_release_from_power_down();
    If this does not work, could you please share all your code Snippet so I can try to reproduce this?

    Kind Regards,
    OV_Renesas

  • Hello,

    I added the release from power down function, but i could not read data from flash.

    Is there any other way to read data from flash memory?

    now since I know the flash location, i.e. 0x0000BD80 , can I use memcpy(); ?

    If possible what is the address that can be used?

  • Hi Sumo,

    Thank you for the reply.
    Could you kindly share your code snippet for handling the SPI Flash?
    Could you also clarify if you are trying to read/write/erase the P25Q11U SPI Flash which is integrated on the DA14531MOD or if you are working with the SPI Flash on the Development Kits?
    After you have read the values from the SPi Flash, you can use memcpy to copy the values to a different variable.

    Kind Regards,
    OV_Renesas