Hello Sir,
I'm using DA14531 as the central. I want to connect two central devices to one peripheral device. Is it possible to implement?
Can we connect multilple central to one peripheral ?
Please clarify the same!!
Thanks in advance!!!
Hi MA,
Thank you for posting your question online.Is the peripheral you are referring to DA14531/DA14531MOD?Please refer on our Multi-Peripheral Example on our GitRepo: BLE_SDK6_examples/connectivity/multi_con_periph at main · dialog-semiconductor/BLE_SDK6_examples · GitHubAs you can see on the readme file, it is possible to configure the DA14531 in order to connect up to 3 central devices. Kind Regards,OV_Renesas
Hello Sir/madam
In this example, Is it possible to vary the advertising name after establishing each connection?
Hi MA,Thank you for the reply and apologies for the delay.Unfortunately, I do not think it is possible to have a different advertising name for each connection. Kind Regards,OV_Renesas