DA 14531 - SUOTA

Hello Sir/Madam

          I'm using DA14531 as the central device. I want to change the connecting device name using the SUOTA.

          I'm following the below link as the reference,

         http://lpccs-docs.renesas.com/Tutorial-BLE-SUOTA-DA145x/introduction.html

          Is it possible to update the software using OTA  in the central role ?

         If it possible means, How can I configure the  central device in  Dialog's SUOTA  app?