mobile application development da1453x

Hi Team,

I am working using da14531 to develop the ibeacon application which is running based on Android Apps. 
The same iOS based beacon scanner app is not recognized with our da14531 module. Will there be any changes required for android or iOS in terms of stack or user app level? Not seen any MAC and not shown the ibeacon message like android.
Is there any specific IOS app required for the da14531 beacon application.
Regards,
Lf
  • Hi Lf,

    Thank you for posting your question online.
    Can you clarify which IOS beacon scanner app and which Android beacon scanner app you are referring to?
    Are you able to find your device via Smartbond App on Android and IOS?
    If you have set the ibeacon format on your Advertising Data you should be able to see your ibeacon data on both Android and IOS.

    Kind Regards,
    OV_Renesas

  • Hi,

    Thanks for your response.,

    I checked with Smartbond in Android it is showing my advertising data in ibeacon with Device name, MAC, UUID, maj and minor fields are showing it is fine.

    But using iOS the same info is not showing in iOS mobile only showing device name and not showing MAC, UUID is showing different, Major and minor fields. why?

    Regards,

    Lf

  • Hi Lf,

    Thank you for the reply.
    Could you share screenshots from both Android and IOS?

    Kind Regards,
    OV_Renesas