BLE+ADC

Hi,

I want to read the ADC value and send it over BLE to mobile app at every 5sec, which BLE peripheral code i need to use , Please suggest asp.

Thanks in Advance

Pavan S K

Parents Reply Children
  • Hi ,

    Its only peripheral example, How to send the ADC value over BLE to mobile app. Which BLE peripheral program to use and how to add adc peripheral there. Please help to share the example program.

    T

  • Hi Pavan,

    I worked on the ble_app_peripheral example.
    The ble_app_peripheral example has by default 3 custom services with multiple custom characteristics.
    If you want more information on how you can achieve that please check this tutorial: DA145XX Tutorial Create a Custom GATT Profile — DA145XX Tutorial Create a Custom GATT Profile (renesas.com)
    In the 1st custom service, there is a characteristic with a Characteristic User Description: "Control Point" and another characteristic with a Characteristic User Description: "ADC Value 1". 
    If you write any value other than 0 on the Control Point characteristic, then a timer starts and updates the ADC Value 1 characteristic every second with an incrementing value.
    On user_custs1_impl.c 
    For the Control Point Characteristic:

    void user_svc1_ctrl_wr_ind_handler(ke_msg_id_t const msgid,
                                          struct custs1_val_write_ind const *param,
                                          ke_task_id_t const dest_id,
                                          ke_task_id_t const src_id)
    {
        uint8_t val = 0;
        memcpy(&val, &param->value[0], param->length);
    
        if (val != CUSTS1_CP_ADC_VAL1_DISABLE)
        {
            timer_used = app_easy_timer(APP_PERIPHERAL_CTRL_TIMER_DELAY, app_adcval1_timer_cb_handler);
        }
        else
        {
            if (timer_used != EASY_TIMER_INVALID_TIMER)
            {
                app_easy_timer_cancel(timer_used);
                timer_used = EASY_TIMER_INVALID_TIMER;
            }
        }
    }

    For the ADC Value 1 Characteristic:
    void app_adcval1_timer_cb_handler()
    {
        struct custs1_val_ntf_ind_req *req = KE_MSG_ALLOC_DYN(CUSTS1_VAL_NTF_REQ,
                                                              prf_get_task_from_id(TASK_ID_CUSTS1),
                                                              TASK_APP,
                                                              custs1_val_ntf_ind_req,
                                                              DEF_SVC1_ADC_VAL_1_CHAR_LEN);
    
        // ADC value to be sampled
        static uint16_t sample      __SECTION_ZERO("retention_mem_area0");
        sample = (sample <= 0xffff) ? (sample + 1) : 0;
    		
    
        //req->conhdl = app_env->conhdl;
        req->handle = SVC1_IDX_ADC_VAL_1_VAL;
        req->length = DEF_SVC1_ADC_VAL_1_CHAR_LEN;
        req->notification = true;
    		/*Change the value updated with adc_val_mv */
        memcpy(req->value, &sample, DEF_SVC1_ADC_VAL_1_CHAR_LEN);
    
        ke_msg_send(req);
    
        if (ke_state_get(TASK_APP) == APP_CONNECTED)
        {
            // Set it once again until Stop command is received in Control Characteristic
            timer_used = app_easy_timer(APP_PERIPHERAL_CTRL_TIMER_DELAY, app_adcval1_timer_cb_handler);
        }
    }

    So, following the Tutorial for GPADC I shared on my previous answer, I added the following code snippets.
    On user_periph_setup.h
    /****************************************************************************************/
    /* UART2 configuration                                                                  */
    /****************************************************************************************/
    // Define UART2 Tx Pad
    #if defined (__DA14531__)
        #define UART2_TX_PORT           GPIO_PORT_0
        #define UART2_TX_PIN            GPIO_PIN_5
    #else
        #define UART2_TX_PORT           GPIO_PORT_0
        #define UART2_TX_PIN            GPIO_PIN_4
    #endif
    
    
    #define ADC_INPUT_PORT                  GPIO_PORT_0
    #define ADC_INPUT_PIN                   GPIO_PIN_6

    On user_periph_setup.c file:
    void GPIO_reservations(void)
    {
    /*
        i.e. to reserve P0_1 as Generic Purpose I/O:
        RESERVE_GPIO(DESCRIPTIVE_NAME, GPIO_PORT_0, GPIO_PIN_1, PID_GPIO);
    */
    
    #if defined (CFG_PRINTF_UART2)
        RESERVE_GPIO(UART2_TX, UART2_TX_PORT, UART2_TX_PIN, PID_UART2_TX);
    #endif
    
        RESERVE_GPIO(LED, GPIO_LED_PORT, GPIO_LED_PIN, PID_GPIO);
    
    #if !defined (__DA14586__)
        RESERVE_GPIO(SPI_EN, SPI_EN_PORT, SPI_EN_PIN, PID_SPI_EN);
    #endif
    	RESERVE_GPIO(ADC_INPUT, ADC_INPUT_PORT, ADC_INPUT_PIN, PID_ADC);
    	
    }
    
    void set_pad_functions(void)
    {
    /*
        i.e. to set P0_1 as Generic purpose Output:
        GPIO_ConfigurePin(GPIO_PORT_0, GPIO_PIN_1, OUTPUT, PID_GPIO, false);
    */
    
    #if defined (__DA14586__)
        // Disallow spontaneous DA14586 SPI Flash wake-up
        GPIO_ConfigurePin(GPIO_PORT_2, GPIO_PIN_3, OUTPUT, PID_GPIO, true);
    #else
        // Disallow spontaneous SPI Flash wake-up
        GPIO_ConfigurePin(SPI_EN_PORT, SPI_EN_PIN, OUTPUT, PID_SPI_EN, true);
    #endif
    
    #if defined (CFG_PRINTF_UART2)
        // Configure UART2 TX Pad
        GPIO_ConfigurePin(UART2_TX_PORT, UART2_TX_PIN, OUTPUT, PID_UART2_TX, false);
    #endif
    		GPIO_ConfigurePin(ADC_INPUT_PORT, ADC_INPUT_PIN, INPUT, PID_ADC, false);
    
        GPIO_ConfigurePin(GPIO_LED_PORT, GPIO_LED_PIN, OUTPUT, PID_GPIO, false);
    }

    On user_custs1_impl.c file:
    #include "adc.h"
    #include "adc_531.h"
    #include "arch_console.h"
    
    /* According to SDK6 Peripheral Drivers Tutorial
     http://lpccs-docs.renesas.com/da145xx_tutorial_sdk6_peripherals/da14531_adc.html
    */
    static uint16_t gpadc_read(void);
    static uint16_t gpadc_sample_to_mv(uint16_t sample);
    
    static uint16_t gpadc_read(void)
    {
        /* Initialize the ADC */
        adc_config_t adc_cfg =
        {
            .input_mode = ADC_INPUT_MODE_SINGLE_ENDED,
            .input = ADC_INPUT_SE_P0_6,
            .smpl_time_mult = 2,
            .continuous = false,
            .interval_mult = 0,
            .input_attenuator = ADC_INPUT_ATTN_4X,
            .chopping = false,
            .oversampling = 0,
        };
        adc_init(&adc_cfg);
    
        /* Perform offset calibration of the ADC */
        adc_offset_calibrate(ADC_INPUT_MODE_SINGLE_ENDED);
    
        adc_start();
        uint16_t result = adc_correct_sample(adc_get_sample());
        adc_disable();
    
        return (result);
    }
    
    static uint16_t gpadc_sample_to_mv(uint16_t sample)
    {
        /* Resolution of ADC sample depends on oversampling rate */
        uint32_t adc_res = 10 + ((6 < adc_get_oversampling()) ? 6 : adc_get_oversampling());
    
        /* Reference voltage is 900mv but scale based in input attenation */
        uint32_t ref_mv = 900 * (GetBits16(GP_ADC_CTRL2_REG, GP_ADC_ATTN) + 1);
    
        return (uint16_t)((((uint32_t)sample) * ref_mv) >> adc_res);
    }

    And on the same file for the ADC Value 1 Characteristic I modified the handler as shown below:
    void app_adcval1_timer_cb_handler()
    {
        struct custs1_val_ntf_ind_req *req = KE_MSG_ALLOC_DYN(CUSTS1_VAL_NTF_REQ,
                                                              prf_get_task_from_id(TASK_ID_CUSTS1),
                                                              TASK_APP,
                                                              custs1_val_ntf_ind_req,
                                                              DEF_SVC1_ADC_VAL_1_CHAR_LEN);
    
        // ADC value to be sampled
        static uint16_t sample      __SECTION_ZERO("retention_mem_area0");
        sample = (sample <= 0xffff) ? (sample + 1) : 0;
    		
    	  /* Perform single ADC conversion */
        uint16_t result = gpadc_read();
    		/* Print the Adc Result */
        arch_printf("\n\radc result: %dmv", gpadc_sample_to_mv(result));
    		/* Save the ADC Result in a variable in order to update the characteristic */
    		uint16_t adc_val_mv = gpadc_sample_to_mv(result);
    
        //req->conhdl = app_env->conhdl;
        req->handle = SVC1_IDX_ADC_VAL_1_VAL;
        req->length = DEF_SVC1_ADC_VAL_1_CHAR_LEN;
        req->notification = true;
    		/*Change the value updated with adc_val_mv */
        memcpy(req->value, &adc_val_mv, DEF_SVC1_ADC_VAL_1_CHAR_LEN);
    
        ke_msg_send(req);
    
        if (ke_state_get(TASK_APP) == APP_CONNECTED)
        {
            // Set it once again until Stop command is received in Control Characteristic
            timer_used = app_easy_timer(APP_PERIPHERAL_CTRL_TIMER_DELAY, app_adcval1_timer_cb_handler);
        }
    }

    Then I build and run the project. When you write any value on the Control Point characteristic you should see the value of the ADC (on P0_6) being updated every 1 second on the ADC Value 1 characteristic.


    Kind Regards,
    OV_Renesas