Hello,
I want to design an application that advertises for X seconds. then stops advertising for Y seconds. then again starts advertising. I am trying to implement the same using app_easy_timer();
as it is visible from the image, I have called stop_advertising_cb().
in the stop advertising call back fuction I have stopped advertising using app_easy_gap_advertise_stop();
Which is working fine. I can also see the next line printed on my uart consol.
Then I have initialised the same timer handler with,
start_advertising_again_cb();
which is not working.
Have I missed something. I have currently set 10s in app_easy_timer();
Hi Sumo,Thank you for posting your question online.When you call the app_easy_gap_advertise_stop function, the app_on_adv_undirect_complete callback function will be called. So, for my implementation I worked…
Hi Sumo,Thank you for posting your question online.When you call the app_easy_gap_advertise_stop function, the app_on_adv_undirect_complete callback function will be called. So, for my implementation I worked on the ble_app_peripheral example and I declared the following:On user_callback_config.h file:
.app_on_adv_undirect_complete = user_app_adv_undirect_complete,
// Default Handler Operations static const struct default_app_operations user_default_app_operations = { .default_operation_adv = user_app_adv_start, //user_app_adv_start };
timer_hnd app_adv_timeout_timer_used __SECTION_ZERO("retention_mem_area0"); #define START_ADV_IN_SEC 500 //5 seconds #define STOP_ADV_IN_SEC 1000 // 10 seconds
app_adv_timeout_timer_used = EASY_TIMER_INVALID_TIMER;
void user_app_adv_start(void) { // Schedule the next advertising data update app_adv_data_update_timer_used = app_easy_timer(APP_ADV_DATA_UPDATE_TO, adv_data_update_timer_cb); struct gapm_start_advertise_cmd* cmd; cmd = app_easy_gap_undirected_advertise_get_active(); // Add manufacturer data to initial advertising or scan response data, if there is enough space app_add_ad_struct(cmd, &mnf_data, sizeof(struct mnf_specific_data_ad_structure), 1); //Check if Timer for Advertising is unitiliazed and initialize him again if( app_adv_timeout_timer_used != EASY_TIMER_INVALID_TIMER) { app_adv_timeout_timer_used = EASY_TIMER_INVALID_TIMER; } // Start the timer to stop advertising after 10seconds app_adv_timeout_timer_used = app_easy_timer(STOP_ADV_IN_SEC, stop_adv_cb); arch_set_extended_sleep(false); app_easy_gap_undirected_advertise_start(); }
void stop_adv_cb(void) { //Check if Timer for Advertising is unitiliazed and initialize him again if( app_adv_timeout_timer_used != EASY_TIMER_INVALID_TIMER) { app_adv_timeout_timer_used = EASY_TIMER_INVALID_TIMER; } app_easy_gap_advertise_stop(); }
void user_app_adv_undirect_complete(uint8_t status) { // If advertising was canceled then wait 5 seconds and start advertising again if (status == GAP_ERR_CANCELED) { app_adv_timeout_timer_used = app_easy_timer(START_ADV_IN_SEC, user_app_adv_start); } }
Thank you!
I am now able to advertise for a specific period of time. Thank you for the solution and explanation.