Hi,
I am doing the advertisement one second interval and the advertisement mode is in connectable mode. sometimes when i am scanning the beacons there is no uuid bytes in the advertisement not even the major minor bytes only the length of 10 bytes its changing. but i never stopping the advertisement and starting that time , still its changing automatically .
please check is something wrong in this.
Thanks,
Sowmiya
Hi Sowmiya,Thank you for posting your question online and apologies for the delay.You have placed this question on the Bluetooth Forum instead of the Bluetooth Low Energy Forum. Let me move this to the BLE Forum.Regarding the change on the advertising data:1) Which BLE device are working with? Is it DA14531?2) Which SDK version are you working with?If you are using DA14531 and the default ibeacon example (from GitRepo) then it is expected the Advertising Data to change. There is an app_easy_timer that expires after 30 seconds that updates the Advertising Data.Best Regards,OV_Renesas
Hi ,
Thanks for the reply ,
One more query from this BLE advertising , can we use the Ibeacon advertisement format with connectable mode ?
https://community.renesas.com/wireles-connectivity/f/bluetooth-low-energy/30092/ibeacon-abvertisemt-not-working-in-changing-of-connectable-mode
This was the link which i have queried before . is this method is possible now ?