Error: L6218E: Undefined symbol arch_asm_delay_us

Hi,

I'm trying to compile an example project (simple_button) from BLE_SDK6_examples (github.com/dialog-semiconductor/).

I have already the SDK installed and I have executed the python script as suggested (python dlg_make_keil5_env_v2.py -sdkpath “<path to your sdk repository>”).

When I try to compile the project it says the following error:

Rebuild started: Project: simple_button
*** Using Compiler 'V6.21', folder: 'C:\Keil_v5\ARM\ARMCLANG\Bin'
Rebuild target 'Simple_Button_531'
compiling exceptions.c...
assembling startup_DA14531.s...
compiling uart_utils.c...
compiling systick.c...
compiling system_DA14531.c...
compiling user_periph_setup.c...
compiling syscntl.c...
compiling main.c...
compiling otp_cs.c...
compiling gpio.c...
compiling hw_otpc_531.c...
compiling uart.c...
compiling arch_system.c...
linking...
.\out_DA14531\Objects\simple_button_531.axf: Error: L6218E: Undefined symbol arch_asm_delay_us (referred from uart.o).
Not enough information to list image symbols.
Not enough information to list load addresses in the image map.
Finished: 2 information, 0 warning and 1 error messages.
".\out_DA14531\Objects\simple_button_531.axf" - 1 Error(s), 0 Warning(s).
Target not created.
Build Time Elapsed: 00:00:01

I don't know what to do to remove this error.

Can someone help me?

Thanks.

Best regards

Parents Reply Children