Hi,
I'm trying to compile an example project (simple_button) from BLE_SDK6_examples (github.com/dialog-semiconductor/).
I have already the SDK installed and I have executed the python script as suggested (python dlg_make_keil5_env_v2.py -sdkpath “<path to your sdk repository>”).
When I try to compile the project it says the following error:
Rebuild started: Project: simple_button*** Using Compiler 'V6.21', folder: 'C:\Keil_v5\ARM\ARMCLANG\Bin'Rebuild target 'Simple_Button_531'compiling exceptions.c...assembling startup_DA14531.s...compiling uart_utils.c...compiling systick.c...compiling system_DA14531.c...compiling user_periph_setup.c...compiling syscntl.c...compiling main.c...compiling otp_cs.c...compiling gpio.c...compiling hw_otpc_531.c...compiling uart.c...compiling arch_system.c...linking....\out_DA14531\Objects\simple_button_531.axf: Error: L6218E: Undefined symbol arch_asm_delay_us (referred from uart.o).Not enough information to list image symbols.Not enough information to list load addresses in the image map.Finished: 2 information, 0 warning and 1 error messages.".\out_DA14531\Objects\simple_button_531.axf" - 1 Error(s), 0 Warning(s).Target not created.Build Time Elapsed: 00:00:01
I don't know what to do to remove this error.
Can someone help me?
Thanks.
Best regards
Hi Javier,Thank you for the reply.
Javi said:I have the USB Dev Kit, now I can debug with Keil but cannot flash when using SmartBond Flash Programmer:
I have the USB Dev Kit, now I can debug with Keil but cannot flash when using SmartBond Flash Programmer:
From the screenshot you shared I see that there are no devices being detected via JTAG interface.Could you please refer on my previous answer when I thought you originally were working with the USB Dev Kit?Have you set the Dip Switch configuration accordingly for SWD?DIP Switch 10 and 11 are for the SWD interface. On the UM-B-125 you can find different DIP switch configurations for UART programming, SWD programming, debug etc.Best Regards,OV_Renesas
Picture updated, DIP switch 1 to 5 ON, 6 to 9 are OFF, 10 to 12 are ON.
Hi Javier,Thank you for updating the picture.It seems that you are able to detect the SWD interface and the DA14531.Could you please try multiple times to see if you are able to erase the Flash?Best Regards,OV_Renesas
It seems that it has been programmed after several tries:
I will try to connect the cables from the USB Dev Kit to my board.
Best regards,
Javier
Hi Javier,Glad you were able to program the USB Dev Kit.If you want to use your USB Dev Kit to program your custom board, please refer here:19. Serial Wire Debug Probe — DA145XX Tutorial SDK Getting started (renesas.com)Best Regards,OV_renesas
Thanks a lot for your help, the link is useful. I've been able to debug DA14531MOD from the USB Dev Kit with cables connected to my board.Now I'm having problems when trying to program the device. After several tries, the program is loaded:
I have checked connections and everything seems fine. I have removed R3 and R11 from USB Dev Kit and connected GND, 3V3, SWDIO and SWCLK to my board, DIP switch from 1 to 9 are OFF and from 10 to 12 are ON. I'm able to debug and sometimes the device can be programmed.
Do you have any clue why this is happening?
Javi said:Thanks a lot for your help, the link is useful. I've been able to debug DA14531MOD from the USB Dev Kit with cables connected to my board.
Glad you were able to debug and program your custom board via the USB Dev Kit.
Javi said:I'm able to debug and sometimes the device can be programmed. Do you have any clue why this is happening? Thanks.
I'm able to debug and sometimes the device can be programmed.
The Renesas SmartBond Flash Programmer is a Development Tool and not a Production tool.Unfortunately, we can not guarantee that it is going to work 100% of the time while testing.The issues you are witnessing should be related to noise on the SWD lines. Please use as small as possible (in length) wires to connect the custom board with the SWD interface on the USB Dev Kit.You can also try to work with the SmartSnippets Toolbox. It requires some more steps in order to program a device, but on the Log window you can receive debug messages that would make us understand why the programming might have failed.Best Regards,OV_Renesas