Questions on DA14531 application

I want to make a gadgets based on DA14531,intergrated with external flash , eInk display and some keys.

This is my first time to use these chips/peripheral, mybe missed some restriction,so,welcome any advices.

These are the basic ideas:

1) DA14531 as application MCU & wireless function provider;

2) eInk as displayer;

3) application code stored in external flash(maybe burn into OTP later, up to the FW size);

4) build keyBoard with ADC function;

    This is not confirmed till now.

   I hope I can use keyBoard controller ,GPIO interrupt and ADC together.

   There is a pivotal question: Is interrupt function available when the PIN set as analog input mode?

   I did not find clear info stating this in DA14531 datasheet.

   Extend I/O inputs is needed for the I/O is not so much for DA14531.

5) external flash & eInk share the SPI bus together with different CS pin;

6) RESET assigned with separate pin(defalut pin P0_0);

The SPI bus will be busy during app running,so we can't let RESET share same pin with SPI bus like USB dongle.scsch

7) app will support central and client at the same time;

4 gadgets cooperate together, anyone of them works in central mode,the remainning in client mode;

8) the design based on design of USB dongle,antenna will use design of Dialog;

9) eInk part copied from design of vendor. 

Why can't I upload .sch file? origal .sch file zipped with winrar:da14531.rar

Parents
  • Hi Xiao,

    Thank you for posting your question online and for your interest in our Wireless Solutions.

    1) DA14531 as application MCU & wireless function provider;

    2) eInk as displayer;

    We do not provide any examples or demo with an eInk as a displayer for the DA14531. 
    Please keep in mind that the total FW size should be less 48kB since DA14531 has 48kB of RAM.
    From that, 8KB are reserved for the BLE stack so you are left with close to 40KB for application code and data. From these 40KB not all can be user code, as a part is taken by the SDK, how large this part is depending on what functionalities you choose to include from the SDK. All things considered the space available for SDK + user code is approximately 40KB.
    I am not sure if this eInk module requires any libraries to run on the DA14531 side, but you should check the firmware size. 
    If the firmware size ends up being an issue, you can refer on our: DA14585 - SmartBondTm Bluetooth 5.0 SoC with Audio Interface | Renesas which is supported by the same SDK and double the RAM (96kB) of DA14531.
    You can also refer on our DA14695 - Multi-Core Bluetooth® 5.2 SoC with System Power Management Unit | Renesas which is way more powerful and we provide examples for LCD modules.


    4) build keyBoard with ADC function;

        This is not confirmed till now.

       I hope I can use keyBoard controller ,GPIO interrupt and ADC together.

       There is a pivotal question: Is interrupt function available when the PIN set as analog input mode?

    It depends on what kind of interrupt functionality you are interested in.
    By default, the ADC driver provides the option for ADC interrupt based on the GPIO you have selected for the GPADC:

    /**
     ****************************************************************************************
     * @brief Registers a callback function to be called within ADC_Handler.
     * @note Enables the ADC_IRQn interrupt.
     * @param[in] callback The callback function.
     ****************************************************************************************
     */
    void adc_register_interrupt(adc_interrupt_cb_t callback);
    
    /**
     ****************************************************************************************
     * @brief Unregisters the callback function that was previously registered.
     * @note Disables the ADC_IRQn interrupt.
     ****************************************************************************************
     */
    void adc_unregister_interrupt(void);
    

    However, if you are referring on a scenario where this interrupt will wake-up the system from sleep, that would not be possible.
    All the peripherals are OFF during any sleep mode. So the GPADC should be shut down during sleep. You can explicitly configure the analog GPIO you want on the wake-up controller to wake-up the device from sleep and then re-configure it as a GPADC GPIO.


    7) app will support central and client at the same time;

    4 gadgets cooperate together, anyone of them works in central mode,the remainning in client mode;

    Please refer on our Multirole example: BLE_SDK6_examples/connectivity/multirole at main · dialog-semiconductor/BLE_SDK6_examples (github.com)

    8) the design based on design of USB dongle,antenna will use design of Dialog;

    9) eInk part copied from design of vendor. 

    Regarding the Schematic you shared:
    Please refer on the AN-B-088: DA145xx Flash Selector Guide (renesas.com)

    On your design you have the G25D40ETIG, but on the List of Supported 3rd Part Flash devices is the G25WD40CTIG. Please make sure that the SPI Flash you have selected is the supported one.

    On the P1 (programming) header you should also expose P0_3 or P0_5 for the 1-wire UART programming option.
    In case your device hangs up during Sleep or if you have remapped the SWD GPIOs then you will not be able to access the SPI Flash via SWD interface.
    The P0_3 or P0_5 can be used in the DA14531 SoC (with the P0_0 HW Reset GPIO) for 1-Wire UART Programming.

    Please also refer on the following:
    AN-B-075: DA14530/531 Hardware Guidelines (renesas.com)
    DA14531 Hardware Design Examples — DA14531 Hardware Design Examples (renesas.com)

    You have selected the Buck mode power configuration:

    You do not have the same values for C1 and C2 on your design.

    Please also check on AN-B-075, section 3.2.2 XTAL, 32MHz, page: 21


    By selecting one of the already tested crystals you can accelerate the time of the design.

    P0_1, P0_6 and P0_7 can be used as GPADC GPIOs, so there is no issue.

    Best Regards,
    OV_Renesas

  • I'm just trying to compile it to make sure configure is right.

    After complete the SDK6patch.diff, I get these errors/warnnings:

    And these changes cause error(examples can be complied without error before trigger error now:      #error "Cannot use ROM app task symbols if number of connections is greater than 1. looks like the patch fix failed)[ solved with preprocessor symbol: __EXCLUDE_ROM_APP_TASK__ ]

    Select device:DA14531

    select AC5

    compile,I get these errors & warnings:

    Many of them.

    But the files exist:

    I have compared with other examples(can compile successfuly),the sets on this site is different:

    This example:

    -mthumb -c -include da1458x_config_basic.h -include da1458x_config_advanced.h -include user_config.h

    others:

    --thumb -c --preinclude da1458x_config_basic.h --preinclude da1458x_config_advanced.h --preinclude user_config.h --bss_threshold=0 --feedback=".\unused_531.txt"

    Change -mthumb to --thumb:

    The error should be triggered by pre warnnings.

    I don't know if I made mistake in those steps or there are other action I should take.

  • Hi Xiao,

    Thank you for the reply.

    But I do not get the reason. The PINs are default,SWD should work if cold start / hardware reset triggered.

    Please refer here: 5. Booting (renesas.com)
    When you do a hardware reset, you will have a few ms before the SWD interface is disabled again from the firmware. We have to recommend to have P0_3 or P0_5 exposed for UART programming. It is up to you, if you want to actually expose them.

    The inductor value placed between VBAT_LOW and LX should be exactly 2.2uH or any bigger one is fine?

    Please refer on our: AN-B-075: DA14530/531 Hardware Guidelines (renesas.com)
    According to the document, the inductor should be 2.2uH.


    I'm just trying to compile it to make sure configure is right.

    After complete the SDK6patch.diff, I get these errors/warnnings:

    From my understanding you are trying to use SDK v6.0.16.
    All our Git examples have been ported into SDK v6.0.18. 
    This is why the patch can not be applied on the SDK v6.0.16.
    I have uploaded the modified SDKs (v6.0.14, v6.0.16, v6.0.18 and v6.0.20) for the Multirole example.
    Please work with these:

    Please download files from the following URL:
    <https://upload.hdedrive.com/ui/renesas.com/dl/SB1707990972-1b06db38-1b58-4d05-9cf4-8df229107312>

    * This URL requires guest identity verification as well as download password authentication.
    Once the identity verification passed, the verification step can be skipped for up to 30 days in the same browser.

    Download Password: K&^!2^ji9LPB

    This URL will expire on February 29, 2024 11:56 AM (UTC+02:00)

    Best Regards,
    OV_Renesas

  • Thank you very much for your help.

    When you do a hardware reset, you will have a few ms before the SWD interface is disabled again from the firmware.

    Yes,I got the reason, hardware has been controlled by bootROM after reset, there is a short time for SWD to take over, after that enter boot loop. The chip maybe be blocked by wrong code.

    I have uploaded the modified SDKs (v6.0.14, v6.0.16, v6.0.18 and v6.0.20) for the Multirole example.

    You are so kind.

    It can be compiled by AC6 now(SDK6.0.20),that is great.

    Thank you.

Reply
  • Thank you very much for your help.

    When you do a hardware reset, you will have a few ms before the SWD interface is disabled again from the firmware.

    Yes,I got the reason, hardware has been controlled by bootROM after reset, there is a short time for SWD to take over, after that enter boot loop. The chip maybe be blocked by wrong code.

    I have uploaded the modified SDKs (v6.0.14, v6.0.16, v6.0.18 and v6.0.20) for the Multirole example.

    You are so kind.

    It can be compiled by AC6 now(SDK6.0.20),that is great.

    Thank you.

Children
No Data