DA14531 Bluetooth version

I follow this tutorial for DA14531.

12. ダイナミック広告データ — DA145XX Tutorial SDK はじめに (renesas.com)

I wanted to use DA14531 for advertising only and was able to see that it sent GAP_AD_TYPE_SERVICE_128_BIT_DATA.
However, since I want to send about 250 bytes of data, I want to switch to Bluetooth5.0 to increase the amount of data I can send.
Where can I set the Bluetooth version?

Parents
  • Hi Yoshihiko-san,

    Thank you for posting your question online.

    Where can I set the Bluetooth version?

    The BLE Core on the DA14531 is based on the Bluetooth SIG Core Specification v5.1. It contains all the mandatory features of the Core Specification v5.1 but not all the optional features offered.

    However, since I want to send about 250 bytes of data, I want to switch to Bluetooth5.0 to increase the amount of data I can send.

    You are not going to be able to send 250 bytes of data via the Advertising Data. 
    Advertising data consists of 31 bytes which 3 of them are reserved for flags on Connectable Advertising. You can also use the Scan Response Data which also consists of 31 bytes. 
    If you want to send 250 bytes of data, you will have to establish a BLE connection and then send those data via a Characteristic.

    Best Regards,
    OV_Renesas

  • Thank you for your reply.

    On the Bluetooth5 page, it says "Extended advertising allows packets to be up to 255 octets long. " but is it possible to use this function?

    Bluetooth_5-FINAL.pdf (Look at P15)

Reply Children