Hi,
This is Abishekh. We are working with DA14695MOD on our custom board with Smartsnippets Studio 2.0.20.4060 and SDK_10.0.12.146.2.
I would like to program one parameter (Size preferred: 8 bytes) - Serial Number in the NVParam section. Basically an unique number for each product, like a running serial number(We do not want to use the mac address). and that information should be available in the code as advertisement parameter.
Can you walk me through how I can achieve this cuz I did not find any guide on adding Nvparam for DA1469X, or any other possible solution for my requirement?
Regards,
Abishekh
Hi Abishekh,
You can follow these params initializations and read api for your using.
BR,
JH_Renesas
Hi, How to add new parameters?
You can append below the IRK data.
BR,JH_Renesas
When I added new data and tried to program it using program_qspi_nvparam, I get Error Jlink.exe not found
But program_qspi_jtag works without issues
I will have a test on this and back to you as soon as possible.
this can help I have tested without error.