DA14695MOD - NVPARAM Usage

Hi,

This is Abishekh. We are working with DA14695MOD on our custom board with Smartsnippets Studio 2.0.20.4060 and SDK_10.0.12.146.2.

I would like to program one parameter (Size preferred: 8 bytes) - Serial Number in the NVParam section. Basically an unique number for each product, like a running serial number(We do not want to use the mac address). and that information should be available in the code as advertisement parameter. 

Can you walk me through how I can achieve this cuz I did not find any guide on adding Nvparam for DA1469X, or any other possible solution for my requirement?

Regards,

Abishekh

Parents Reply Children
No Data