GPIO wake-up and sleep

Dear Dialog Support,

I am testing the example ble_app_peripheral in SDK_6.0.18.1182.1. I want to realize the following function:

Once DA14531 is powered on, it enters into the extended sleep mode. When the button is pressed down once, DA14531 wakes up and the functions of the original example ble_app_peripheral can normally perform. And when the button is pressed down once again, DA14531 enters into the extended sleep mode again, and so on.

Could you please show me how to achieve this. Thanks a lot!

Parents
  • Hi Nick,

    Thank you for posting your question online.
    Please find attached the ble_app_peripheral_wakeup.zip file. 
    I worked on SDK v6.0.18 with the DA14531MOD and the Dev Kit Pro.
    I configured the P0_11 as my button and whenever I press the button I get into Extended sleep mode or exit Extended Sleep Mode.
    Please refer to this project for your implementation.

    Best Regards,
    OV_Renesas
    ble_app_peripheral_wakeup.zip

  • Dear OV,

    I downloaded your code and tested it, but I failed with my custom board. My board configuration is shown below:

    And I also uploaded the testing video, as you can see, when I used the wire connected to P0.11 to plug the GND on the board, DA14531 seemed enter the extended sleep mode. Actually, the supply current changed from 230uA to tens of uA (17uA to 50uA), but I remember the extended-sleep current should be 3uA. And then I plugged to GND again, DA14531 cannot resume to the active mode. Could you please help to find the problems? Thanks a lot!

  • Dear Nick,

    Thank you for the reply.
    From the video you shared I can see that you are downloading the firmware into the RAM of the DA14531.
    Could you please download the firmware into the SPI Flash and test again? 
    There could be also leakage current from the custom board. Have you made sure you have calibrated the tool you are using for current measurements so it will only get the DA14531 current consumption?

    P.S. I really enjoyed the birds chirping in the background Smiley.

    Best Regards,
    OV_Renesas

Reply
  • Dear Nick,

    Thank you for the reply.
    From the video you shared I can see that you are downloading the firmware into the RAM of the DA14531.
    Could you please download the firmware into the SPI Flash and test again? 
    There could be also leakage current from the custom board. Have you made sure you have calibrated the tool you are using for current measurements so it will only get the DA14531 current consumption?

    P.S. I really enjoyed the birds chirping in the background Smiley.

    Best Regards,
    OV_Renesas

Children
  • Dear OV,

    Thanks for your kindly reply.

    I downloaded the firmware into the SPI Flash, but the result is the same.

    I am sure the tool measures the DA14531 current only. You can confirm this from the start of the video.

    And there is no leakage current from the custom board. I tested the current in the extended sleep mode previously, and it can drop to around 3uA.

    So I am still confused.

    Please continue helping on this. Thanks a lot.

    P.S. I am glad you enjoy the birds chirping in my video. 

    Best regards,

    Nick

  • Hi Nick,

    Thank you for the reply. Apologies for the delay.

    . I tested the current in the extended sleep mode previously, and it can drop to around 3uA.

    In which project had you measured the current consumptuion?

    So I am still confused.

    Please check on the SDK6 Release Notes as well:

    If you do not keep the RAM cells detained you will witness a lower current consumption. However, each time you wake-up from Sleep mode (in Extended Sleep mode, each scan/advertise interval) you will have to load again the FW from the SPI Flash which can affect the current consumption as well.

    Best Regards,
    OV_Renesas

  • Dear OV,

    Thanks for your reply.

    I found the second video was just invalid, and now I updated it. You can see from it that I can only put DA14531 into sleep mode but cannot pull it back to the active state. This is the main problem I need your help now.

    About the sleep current issue, I found why the sleep current is around 17uA. I just made a stupid mistake. I forgot there is a serial communication CH340 IC on my board, and it consume around 15uA. Sorry about that.

    Best regards,

    Nick

  • Dear Nick,

    Thank you for the reply.
    Glad you were able to see the expected current consumption.

    You can see from it that I can only put DA14531 into sleep mode but cannot pull it back to the active state. This is the main problem I need your help now.

    Have you burned the FW into the Flash during the test?
    What is the Flash part number integrated on your Dev Kit?
    Have you made any modifications on the Project I shared?

    Best Regards,
    OV_Renesas

  • Dear OV,

    Have you burned the FW into the Flash during the test?
    What is the Flash part number integrated on your Dev Kit?

    Yes, I have burned the FW into Flash during the test.

    The Flash part number is P25Q40.

    Have you made any modifications on the Project I shared?

    No, I did not modify your codes.

  • Hi Nick,

    Thank you for the reply.
    By default, I used the DA14531MOD which has the P25Q11U part number.
    On user_periph_setup.h file please add the following:

    /****************************************************************************************/
    /* SPI configuration                                                                    */
    /****************************************************************************************/
    // Define SPI Pads
    #if defined (__DA14531__)
        #define SPI_EN_PORT             GPIO_PORT_0
        #define SPI_EN_PIN              GPIO_PIN_1
    
        #define SPI_CLK_PORT            GPIO_PORT_0
        #define SPI_CLK_PIN             GPIO_PIN_4
    
        #define SPI_DO_PORT             GPIO_PORT_0
        #define SPI_DO_PIN              GPIO_PIN_0
    
        #define SPI_DI_PORT             GPIO_PORT_0
        #define SPI_DI_PIN              GPIO_PIN_3
    
    #elif !defined (__DA14586__)
        #define SPI_EN_PORT             GPIO_PORT_0
        #define SPI_EN_PIN              GPIO_PIN_3
    
        #define SPI_CLK_PORT            GPIO_PORT_0
        #define SPI_CLK_PIN             GPIO_PIN_0
    
        #define SPI_DO_PORT             GPIO_PORT_0
        #define SPI_DO_PIN              GPIO_PIN_6
    
        #define SPI_DI_PORT             GPIO_PORT_0
        #define SPI_DI_PIN              GPIO_PIN_5
    #endif
    
    /***************************************************************************************/
    /* Production debug output configuration                                               */
    /***************************************************************************************/
    #if PRODUCTION_DEBUG_OUTPUT
    #if defined (__DA14531__)
        #define PRODUCTION_DEBUG_PORT   GPIO_PORT_0
        #define PRODUCTION_DEBUG_PIN    GPIO_PIN_11
    #else
        #define PRODUCTION_DEBUG_PORT   GPIO_PORT_2
        #define PRODUCTION_DEBUG_PIN    GPIO_PIN_5
    #endif
    #endif
    
    // Define SPI Configuration
        #define SPI_MS_MODE             SPI_MS_MODE_MASTER
        #define SPI_CP_MODE             SPI_CP_MODE_0
        #define SPI_WSZ                 SPI_MODE_8BIT
        #define SPI_CS                  SPI_CS_0
    
    #if defined(__DA14531__)
        #define SPI_SPEED_MODE          SPI_SPEED_MODE_4MHz
        #define SPI_EDGE_CAPTURE        SPI_MASTER_EDGE_CAPTURE
    #else // (DA14585, DA14586)
        #define SPI_SPEED_MODE          SPI_SPEED_MODE_4MHz
    #endif
    #if !defined (__DA14586__)
    #define SPI_FLASH_DEV_SIZE          (512 * 1024)	//for P25Q40 4Mb
    #endif
    

    Please modify the SPI pins based on your board.
    And on user_periph_setup.c file:
    /**
     ****************************************************************************************
     *
     * @file user_periph_setup.c
     *
     * @brief Peripherals setup and initialization.
     *
     * Copyright (C) 2015-2019 Dialog Semiconductor.
     * This computer program includes Confidential, Proprietary Information
     * of Dialog Semiconductor. All Rights Reserved.
     *
     ****************************************************************************************
     */
    
    /*
     * INCLUDE FILES
     ****************************************************************************************
     */
    
    #include "user_periph_setup.h"
    #include "datasheet.h"
    #include "system_library.h"
    #include "rwip_config.h"
    #include "gpio.h"
    #include "uart.h"
    #include "syscntl.h"
    #include "fpga_helper.h"
    
    /*
     * GLOBAL VARIABLE DEFINITIONS
     ****************************************************************************************
     */
    
    /**
     ****************************************************************************************
     * @brief Each application reserves its own GPIOs here.
     ****************************************************************************************
     */
    
    #if DEVELOPMENT_DEBUG
    
    void GPIO_reservations(void)
    {
    /*
        i.e. to reserve P0_1 as Generic Purpose I/O:
        RESERVE_GPIO(DESCRIPTIVE_NAME, GPIO_PORT_0, GPIO_PIN_1, PID_GPIO);
    */
    	    // Push Button
        RESERVE_GPIO(PUSH_BUTTON, GPIO_BUTTON_PORT, GPIO_BUTTON_PIN, PID_GPIO);
    
    #if defined (CFG_PRINTF_UART2)
        RESERVE_GPIO(UART2_TX, UART2_TX_PORT, UART2_TX_PIN, PID_UART2_TX);
    #endif
    
        RESERVE_GPIO(LED, GPIO_LED_PORT, GPIO_LED_PIN, PID_GPIO);
    
    #if defined (CFG_SPI_FLASH_ENABLE)	
    	RESERVE_GPIO(SPI_FLASH_CS, SPI_EN_PORT, SPI_EN_PIN, PID_SPI_EN);
    	RESERVE_GPIO(SPI_FLASH_CLK, SPI_CLK_PORT, SPI_CLK_PIN, PID_SPI_CLK);
    	RESERVE_GPIO(SPI_FLASH_DO, SPI_DO_PORT, SPI_DO_PIN, PID_SPI_DO);
    	RESERVE_GPIO(SPI_FLASH_DI, SPI_DI_PORT, SPI_DI_PIN, PID_SPI_DI);
    #endif
    }
    
    #endif
    
    void set_pad_functions(void)
    {
    /*
        i.e. to set P0_1 as Generic purpose Output:
        GPIO_ConfigurePin(GPIO_PORT_0, GPIO_PIN_1, OUTPUT, PID_GPIO, false);
    */
    
        // Push Button
        GPIO_ConfigurePin(GPIO_BUTTON_PORT, GPIO_BUTTON_PIN, INPUT_PULLUP, PID_GPIO, false);
    	
    #if defined (CFG_SPI_FLASH_ENABLE)
        // Configure SPI pins
        GPIO_ConfigurePin(SPI_EN_PORT, SPI_EN_PIN, OUTPUT, PID_SPI_EN, true);
        GPIO_ConfigurePin(SPI_CLK_PORT, SPI_CLK_PIN, OUTPUT, PID_SPI_CLK, false);
        GPIO_ConfigurePin(SPI_DO_PORT, SPI_DO_PIN, OUTPUT, PID_SPI_DO, false);
        GPIO_ConfigurePin(SPI_DI_PORT, SPI_DI_PIN, INPUT, PID_SPI_DI, false);
        
       
    #endif
    
    #if defined (CFG_PRINTF_UART2)
        // Configure UART2 TX Pad
        GPIO_ConfigurePin(UART2_TX_PORT, UART2_TX_PIN, OUTPUT, PID_UART2_TX, false);
    #endif
    
        GPIO_ConfigurePin(GPIO_LED_PORT, GPIO_LED_PIN, OUTPUT, PID_GPIO, false);
    }
    
    
    
    #if defined (CFG_PRINTF_UART2)
    // Configuration struct for UART2
    static const uart_cfg_t uart_cfg = {
        .baud_rate = UART2_BAUDRATE,
        .data_bits = UART2_DATABITS,
        .parity = UART2_PARITY,
        .stop_bits = UART2_STOPBITS,
        .auto_flow_control = UART2_AFCE,
        .use_fifo = UART2_FIFO,
        .tx_fifo_tr_lvl = UART2_TX_FIFO_LEVEL,
        .rx_fifo_tr_lvl = UART2_RX_FIFO_LEVEL,
        .intr_priority = 2,
    };
    #endif
    
    // Configuration struct for SPI
    const spi_cfg_t spi_cfg = {
        .spi_ms = SPI_MS_MODE,
        .spi_cp = SPI_CP_MODE,
        .spi_speed = SPI_SPEED_MODE,
        .spi_wsz = SPI_WSZ,
        .spi_cs = SPI_CS,
        .cs_pad.port = SPI_EN_PORT,
        .cs_pad.pin = SPI_EN_PIN,
    #if defined (__DA14531__)
        .spi_capture = SPI_EDGE_CAPTURE,
    #endif
    #if defined (CFG_SPI_DMA_SUPPORT)
        .spi_dma_channel = SPI_DMA_CHANNEL_01,
        .spi_dma_priority = DMA_PRIO_0,
    #endif
    };
    
    // Configuration struct for SPI FLASH
    const spi_flash_cfg_t spi_flash_cfg = {
        .chip_size = SPI_FLASH_DEV_SIZE,
    		.jedec_id = P25Q40U_JEDEC_ID,
    		.dev_index = P25Q40U_DEV_INDEX
    };
    void periph_init(void)
    {
    #if defined (__DA14531__)
        // Select FPGA GPIO_MAP 1
        // set debugger SWD to SW_CLK = P0[2], SW_DIO=P0[5]
        FPGA_HELPER(FPGA_GPIO_MAP_1, SWD_DATA_AT_P0_5);
    
        // In Boost mode enable the DCDC converter to supply VBAT_HIGH for the used GPIOs
        // Assumption: The connected external peripheral is powered by 3V
        syscntl_dcdc_turn_on_in_boost(SYSCNTL_DCDC_LEVEL_3V0);
    #else
        // Power up peripherals' power domain
        SetBits16(PMU_CTRL_REG, PERIPH_SLEEP, 0);
        while (!(GetWord16(SYS_STAT_REG) & PER_IS_UP));
        SetBits16(CLK_16M_REG, XTAL16_BIAS_SH_ENABLE, 1);
    #endif
    
        // ROM patch
        patch_func();
    
        // Initialize peripherals
    #if defined (CFG_PRINTF_UART2)
        // Initialize UART2
        uart_initialize(UART2, &uart_cfg);
    #endif
    
    #if defined (CFG_SPI_FLASH_ENABLE)
        // Configure SPI Flash environment
         spi_flash_configure_env(&spi_flash_cfg);
    
        // Initialize SPI
        spi_initialize(&spi_cfg);
    #endif
    
        // Set pad functionality
        set_pad_functions();
    
        // Enable the pads
        GPIO_set_pad_latch_en(true);
    }
    

    Make sure you also define the CFG_SPI_FLASH_ENABLE macro on the da1458x_config_basic.h file and you call the spi_flash_power_down() API on the user_app_init to get the SPI Flash to power down when the application starts. 
    Note: You will need to include the spi_flash.h file in order to do that.

    Then please compile and load the new FW into your board and test again.

    Best Regards,
    OV_Renesas