AT COMMAND IN DA14531

Im using basic AT command in ADA14531. I used AT+GAPCONNECT to connect to certain ble module. however, i cannot set it as central ble or master BLE to allow it to scan for ther ble. do i have to use binary code or what?