DA14531 - add features to prox reporter example

i need to add features like

  • it should bond with only one device (to store the MAC ID 1st time)
  • it should pair with that device (when the mac ID matches)
  • no other device should not be connected in between or bonded with the device

how can i do these things to the prox reporter example