Hi sir,
I made the equipment using da14531 mod.
The MCU and DA14531 we use use UART communication.
DA14531 is applied with DSPS_device f/w. DA14531 is connected to the mobile phone, and eventually, the mobile phone and our equipment are wirelessly communicating.
The problem isThere are hundreds of developed equipment and use basic DSPS_device f/w, so device_name is all the same when searching for a mobile phone (there is a situation where various equipment is turned on in the same space)Of course, you can change device_name through f/w compilation, but you can't compile all of the hundreds of modules.
What I am curious about is the content below.
1. I was wondering if there is a way to change device_name separately in the module except for the compilation tool.
2. Is there a way to read BD address from MCU to UART from MCU connected to uart if number 1 doesn't work? (All communications sent from mcu to uart to da14531 are sent to mobile phone. I don't know how.)
If it is applied as mass production, I don't think it will be our own problem. I wonder if there are any other solutions
thanks
Thanks ,