Issue in DA14531 MOD Bluetooth range

Hi Team,

Iam using CodeLess: 6.380.14.22

In my code i have set power level as +2.5 dBm and working as expected range like 25 to 30 meters.

But the same code is flashed to other Module, which is not working beyond 5 meters.

How do we say it is hardware of DA14531 MOD issue or Firmware issue?

If it is Hardware issue how can we fix it?

How can we check the power level is really set to +2.5dBm?

Regards,

Laxmi Narayana 

Parents Reply
  • Hi Laxmi,

    Thank you for the reply.

    As per Design Guidelines, we have designed and placed DA14531 MOD in our custom board. But still we are facing BT range issue with some modules. 

    Did you follow the same procedure for all the custom boards? How many boards have this issue?
    Did you make sure to follow the Soldering Guidelines as well on section 9 Soldering page 22?
    Would it be possible to remove the DA14531MOD from the custom board and test it separately to see if it has the correct behavior?

    Best Regards,
    OV_Renesas

Children