Hi Team,
Iam using CodeLess: 6.380.14.22
In my code i have set power level as +2.5 dBm and working as expected range like 25 to 30 meters.
But the same code is flashed to other Module, which is not working beyond 5 meters.
How do we say it is hardware of DA14531 MOD issue or Firmware issue?
If it is Hardware issue how can we fix it?
How can we check the power level is really set to +2.5dBm?
Regards,
Laxmi Narayana