DA14531MOD FIRMWARE UPDATE

Hi 

I have DA14531mod which one i want to use it in AT-Command Mode (Codeless) but i recently i got information we need to update firmware of these module so please guide me how i can update the firmware of these using FTD 

also please suggest how i can use it same module with RX71M mcu

  • Hi i am getting these error Please note i am using FT232RL

    [INFO Flash Code@24-05-30 10:29:10] Firmware File C:\Program Files\SmartSnippetsToolbox\SmartSnippetsToolbox5.0.24\common_resources\SupportPackages\DA1453x\toolbox_resources/common/flash_programmer_531.bin has been selected for downloading.
    [INFO Flash Code@24-05-30 10:29:11] Connection to COM60 port has successfully opened.
    [INFO Flash Code@24-05-30 10:29:11] Started download procedure...
    [ACTION Flash Code@24-05-30 10:29:12] Please press the hardware reset button on the board to start the download process.
    [INFO Flash Code@24-05-30 10:29:12] Reset detected
    [ERROR Flash Code@24-05-30 10:29:14] CRC does not match.
    [ACTION Flash Code@24-05-30 10:29:14] Please click the Connect/Download button in SmartSnippets Toolbox and press the hardware reset button on the board to start the download process.
    [INFO Booter@24-05-30 10:29:14] Successfully disconnected from port COM60.
    [ERROR Flash Code@24-05-30 10:29:14] Failed downloading firmware file to the board.
    [INFO Flash Code@24-05-30 10:33:46] Firmware File C:\Program Files\SmartSnippetsToolbox\SmartSnippetsToolbox5.0.24\common_resources\SupportPackages\DA1453x\toolbox_resources/common/flash_programmer_531.bin has been selected for downloading.
    [INFO Flash Code@24-05-30 10:33:46] Connection to COM60 port has successfully opened.
    [INFO Flash Code@24-05-30 10:33:46] Started download procedure...
    [ACTION Flash Code@24-05-30 10:33:47] Please press the hardware reset button on the board to start the download process.
    [INFO Flash Code@24-05-30 10:33:50] Reset detected
    [INFO Booter@24-05-30 10:34:02] Successfully disconnected from port COM60.
    [ERROR Flash Code@24-05-30 10:34:02] Error while sending firmware bytes to FTDI device.
    [ERROR Flash Code@24-05-30 10:34:02] Failed downloading firmware file to the board.

  • yes i followed above connections & steps

    also tried below connection but same result

  • It seems something happed when you press Rest, FTDI device. disconnect:

    Could you post your board connection picture here.

  • hi  ,

    Thanks for the support..

    My problem is solved  but the i was connected (p05/rxtx) pin to tx pin(1) of ft232rl now i am facing issue with AT commands please check below commands & there response & suggest any documents if you have

    11:20:12.139 -> ready
    11:20:18.139 -> AT
    11:20:18.139 ->
    11:20:18.139 -> OK
    11:20:21.935 -> ATE
    11:20:21.935 -> 1
    11:20:21.935 -> OK
    11:20:31.514 -> AT+BINREQ
    11:20:31.514 -> INVALID COMMAND.
    11:20:31.561 -> ERROR
    11:20:38.748 -> AT+CENTRAL
    11:20:38.748 ->
    11:20:38.748 -> ERROR
    11:20:59.624 -> AT+ADVSTOP
    11:20:59.624 ->
    11:20:59.624 -> OK
    11:21:02.811 -> AT+CENTRAL
    11:21:02.858 ->
    11:21:02.858 -> OK
    11:21:13.232 -> AT+PERIPHERAL
    11:21:13.279 ->
    11:21:13.279 -> OK
    11:21:19.967 -> AT+BINREQ
    11:21:19.967 -> INVALID COMMAND.
    11:21:20.014 -> ERROR
    11:21:26.170 -> AT+CENTRAL
    11:21:26.217 ->
    11:21:26.217 -> OK
    11:21:28.029 -> AT+BINREQ
    11:21:28.029 -> INVALID COMMAND.
    11:21:28.029 -> ERROR
    11:21:56.935 -> AT+GAPSCAN
    11:21:56.935 -> SCANNING
    11:21:57.029 ->
    11:21:57.029 -> ( ) 68:E7:4A:EC:0F:32,P, Type: ADV, RSSI:-80
    11:21:57.170 ->
    11:21:57.170 -> ( ) D4:36:39:93:22:1D,P, Type: ADV, RSSI:-70
    11:21:57.217 ->
    11:21:57.217 -> ( ) D4:36:39:93:22:1D,P, Type: RSP, RSSI:-70R:7
    11:21:57.310 -> ( ) E3:4F:A7:E5:C4:88,R, Type: ADV, RSSI:-68
    11:21:57.357 ->
    11:21:57.357 -> ( ) E3:4F:A7:E5:C4:88,R, Type: RSP, RSSI:-67 Px13A5480000000
    11:21:57.593 -> ( ) 52:8B:46:79:92:93,R, Type: ADV, RSSI:-91
    11:21:57.639 ->
    11:21:57.639 -> ( ) 52:8B:46:79:92:93,R, Type: RSP, RSSI:-92
    11:21:57.862 ->
    11:21:57.862 -> ( ) D2:6D:CC:CD:67:57,R, Type: ADV, RSSI:-97
    11:21:58.232 ->
    11:21:58.232 -> ( ) 49:87:7B:3D:D0:B9,R, Type: ADV, RSSI:-91
    11:21:59.012 ->
    11:21:59.012 -> ( ) F5:A7:8E:B4:45:51,R, Type: ADV, RSSI:-94
    11:21:59.059 ->
    11:21:59.059 -> ( ) 49:87:7B:3D:D0:B9,R, Type: ADV, RSSI:-92
    11:21:59.106 ->
    11:21:59.106 -> ( ) 49:87:7B:3D:D0:B9,R, Type: RSP, RSSI:-92
    11:21:59.200 -> ( ) 68:E7:4A:EC:0F:32,P, Type: RSP, RSSI:-77,
    11:21:59.436 ->
    11:21:59.436 -> ( ) F5:A7:8E:B4:45:51,R, Type: ADV, RSSI:-95
    11:22:00.358 ->
    11:22:00.358 -> ( ) D2:6D:CC:CD:67:57,R, Type: ADV, RSSI:-95
    11:22:00.733 ->
    11:22:00.733 -> ( ) 49:87:7B:3D:D0:B9,R, Type: ADV, RSSI:-92
    11:22:00.780 ->
    11:22:00.780 -> ( ) 49:87:7B:3D:D0:B9,R, Type: RSP, RSSI:-92
    11:22:00.999 -> ( ) 49:87:7B:3D:D0:B9,R, Type: ADV, RSSI:-91
    11:22:01.842 ->
    11:22:01.842 -> ( ) 49:87:7B:3D:D0:B9,R, Type: ADV, RSSI:-88
    11:22:01.889 ->
    11:22:01.889 -> ( ) 49:87:7B:3D:D0:B9,R, Type: RSP, RSSI:-8
    11:22:04.607 -> SCAN COMPLETE
    11:22:04.607 -> OK

  • Hi ,

    Thanks again for your support,

    i have one Query about firmware update process

    suppose we update FW by following above process & if we want to again change firmware to  DA14531 Datapump from standalone is it possible with above same process

    ?????

  • yes, one-wire loading firmware have no difference with SWD, only IO configuration not the same.

  • it is not working it not working is it i need to do any change in process or hardware wiring

    Flash Code@24-06-03 08:59:13] Firmware File C:\Program Files\SmartSnippetsToolbox\SmartSnippetsToolbox5.0.24\common_resources\SupportPackages\DA1453x\toolbox_resources/common/flash_programmer_531.bin has been selected for downloading.
    [INFO Flash Code@24-06-03 08:59:13] Connection to COM60 port has successfully opened.
    [INFO Flash Code@24-06-03 08:59:13] Started download procedure...
    [ACTION Flash Code@24-06-03 08:59:14] Please press the hardware reset button on the board to start the download process.
    [ERROR Flash Code@24-06-03 08:59:21] Timeout: Reset signal not detected for more than 8000 msecs.
    [INFO     Flash Code@24-06-03 08:59:21] Please try again. If problem persists refer to User Manual AN-B-072 (www.renesas.com/.../b-072-da14531-booting-otp-and-serial-interfaces) and check jumper settings. For booting from 2-wire UART  (P0_0 and P0_1) see Figure 10. For booting from 1-wire UART P0_5 see Figure 6.
    [INFO Booter@24-06-03 08:59:21] Successfully disconnected from port COM60.
    [ERROR Flash Code@24-06-03 08:59:21] Error while writing to the board.
    [ERROR Flash Code@24-06-03 08:59:21] Failed downloading firmware file to the board.