Additional 100nF capacitance to the DA1469x VSUP_RF pin

Hi,

 

We guess if an additional 100nF capacitance is added to the DA1469x VSUP_RF(V14) pin, the 1V2 LDO of radio which depends on VSUP_RF will be more stable, then the performance of range application will be improved because of the more stable refence voltage for RF ADC.

 

Could you kindly tell us the guess is OK or not? If the additional 100nF capacitance has no obviously bad effect to the range application performance, we want to try.

 

Best regards,

Peter