Additional 100nF capacitance to the DA1469x VSUP_RF pin

Hi,

 

We guess if an additional 100nF capacitance is added to the DA1469x VSUP_RF(V14) pin, the 1V2 LDO of radio which depends on VSUP_RF will be more stable, then the performance of range application will be improved because of the more stable refence voltage for RF ADC.

 

Could you kindly tell us the guess is OK or not? If the additional 100nF capacitance has no obviously bad effect to the range application performance, we want to try.

 

Best regards,

Peter

Parents
  • Hi Peter,

    All our characterization and evaluation is done with 10μF ( ~7μF effective @ DC-Bias = 1.4V) at V14 and VSUP_RF.
    On the characterization boards and the evaluation kits.
    Also, as far as we know, there is no difference in performance when operating on the internal Simo DCDC (ripple) or the internal LDOs (no ripple).
    The RF LDO should give enough isolation/rejection.

    You may try it of course, it will certainly not harm. But we do not believe that you are going to find any improvements.

    Best Regards,
    OV_Renesas

Reply
  • Hi Peter,

    All our characterization and evaluation is done with 10μF ( ~7μF effective @ DC-Bias = 1.4V) at V14 and VSUP_RF.
    On the characterization boards and the evaluation kits.
    Also, as far as we know, there is no difference in performance when operating on the internal Simo DCDC (ripple) or the internal LDOs (no ripple).
    The RF LDO should give enough isolation/rejection.

    You may try it of course, it will certainly not harm. But we do not believe that you are going to find any improvements.

    Best Regards,
    OV_Renesas

Children