Not able to compile L2CAP example.

Hi Team,

To achieve throughput optimization, i want to use L2CAP example as mentioned in below link:

https://github.com/dialog-semiconductor/BLE_SDK6_examples/tree/main/features/dynamic_L2CAP_Packet_size_Optimization

Before compiling i done the sdk environment set-up as suggested in ReadMe.

Below is the Output after running the python script:

Now i opened the project in Keil IDE and tried to compile. Then i am facing linking issue as shown in below screenshot:

Finally i want to integrate this example with CodeLess code to increase the data throughput.

Please help me fixing this issue.

Regards,

Laxmi Narayana.