Does anyone know why the DA14683 would not come out of sleep mode?
We have a setup that from a hardware point of view is identical to the development daughter board DA14684 DB AQFN vD. If we run the code on the daughter board powered on its own by a coin cell it goes to sleep and comes out on the 5seconds on 5 seconds off cycle we have set.
Running the same code on our board it works for a few cycles then stops. Totally baffled, help please.
Hi JeffKAllen,
Thank you for posting your questions online.
1, Which SDK version you are using?
2, You can compare with the EVK schematic: https://www.renesas.com/us/en/document/sch/da14683-pro-development-kit-daughter-board-schematic-aqfn?r=1580551
3, Does the customer board powered the same as EVK?
4, You can share your schematic if it's possible.
BR,
JH_Renesas
Hi JH Thank you or quick response,
1. The SDK version is 1.0.14.1081
2. The schematic is at https://www.dropbox.com/scl/fi/rwocxsxcz5hz7d5lmuu6v/Screenshot-2024-06-13-at-09.25.55.png?rlkey=jzv585dkm083ube290m8ogab2&dl=0
As far as i can see this is near enough identical to the EVK schematic
3. The power is provided on VBAT and is from a 3.7V lithium battery
4. The timer being used is the free RTOS timer provided in the SDK that we believe uses timer 1
BR Jeff
Hi Jeff,
Which sleep mode are you using.
Hi JH Extended sleep mode.
We have yesterday done the following :
On your EVK board put on the firmware to put the unit to sleep for 5 seconds wake for 5 seconds and power it from a power supply on VBAT at 3.8V, current consumption when awake is 1mA when asleep is 20uA which is all as it should be.
We then put the same firmware on our board, the current consumption when awake is 2mA and when asleep goes up to 200uA, but it then never wakes up.
We therefore suspect a hardware issue, but we are certain it cannot be a build issue because we have built the same chip onto 3 different boards and get pretty much the same issue on all the boards
I will send you the PCB layouts please could you take a look and tell me if this could be a layout issue, we have tried to follow your layout but there are minor differences.
Thanks
Jeff
I got updates from HW team:
I have checked the schematic, and found nothing relevant for the issue.One item not related to issue has been found, please see last line in this comment. Some questions to the customer:
JH_Renesas said:The one comment about the SCH: the LED D1 can not work as it's connected like in the schematic. The LED1 pin of the DA14683 is an Open-Drain output. So the LED has to be connected to a supply, e.g. +3V3.
We don't use this so not an issue but will note for future Thank you
Hi JH
JH_Renesas said:what are the following rail voltages when the device is not waking up and the VBAT current is 200 µA? VBAT V33 V18 V18p V14 V12 ? V ? V ? V ? V ? V ? V
Vbat is stable at 3.653
V33 is stable at 3.25V
V18 is stable at 1.795V
V12 is stable at 1.15/1.17V, but drops when unit goes to sleep, when it comes back up after the time period it has a bit more ripple on it
V14 varies depending on state from 1.3V to 1.4V
V18P powers up to 1.8V on power up but then decays to about 0.45V and never comes back up.
Another thing noticed is the power consumption. On power up while running current is 1.9mA approx, when sleep starts current drops to approx 200uA, but then after the 5 seconds sleep time the current goes back up to 1.14mA but the unit does not start up properly, seems it is timing during sleep but not able to power up correctly on trying to leave sleep mode.
JH_Renesas said:so, also at VBAT = 3.8 V from external power supply, the chip is not waking up after some time?
Correct when powered up from an external supply at 3.7 or 3.8V it does not wake up
KR Jeff
JeffKAllen said:Another thing noticed is the power consumption. On power up while running current is 1.9mA approx, when sleep starts current drops to approx 200uA, but then after the 5 seconds sleep time the current goes back up to 1.14mA but the unit does not start up properly, seems it is timing during sleep but not able to power up correctly on trying to leave sleep mode.
On the dev kit board the power consumption is is 1.2mA when running and 20uA when asleep with the same firmware, as with the above the power supplies measure similarly. However after going to sleep and wakinig up for the first time the power comes back to 900uA not 1.2mA
Hi Jeff, Thanks for your info.
1, Q: what is status of the low-power Xtal32K oscillator? The lower power consumption after waking up the first time can be explained I think: When booting, the chip is operating on the internal LDOs, until first time going into sleep-mode. After that, the more efficient DCDC is used, and VBAT current will be lower than when using the LDOs (0.9 mA vs. 1.2 mA).
2,
the issue appearing after waking up the first time and using the DCDC makes me think of following:
- PCB design comments:
3, As a test, manually a copper-foil connection could be made (soldered) from one side of the ground to the other side of the ground. Use some wide copper foil to make a more solid ground area.
Yes the board is 2 layer, but we also have the same issue on a 4 layer version.
The 32kHz crystal is running
We have tried disabling the DCDC and now all seems to work, i am becoming convinced this is grounding issue, so looks like we will have to go to 4 layers to solve the issues.
Would you be able to review gerbers before we commit?
Thoughts?
Hi JH, have redone the artwork
This is the ground plane inner layer for the new artwork
This is the new bottom layer artwork, yo will see the vias for the ground connections
I am hoping this will sort the issues, any comments gratefully received.
Is this 4 layers board? but same top/bottom You can share the file or screenshot to my email.
I will share with our HW team for review.
Jason
Have sent you the files
Hi Jason
We have built first boards modified as specified, except for these first ones do not have the ground planes open beneath the crystal oscillator active pads as you suggested. The next ones do have this change. In meantime we tested the boards, all is working as expected, except for the current consumption in extended sleep mode this is still at 170 to 200uA, any ideas on what this could be caused by, could it be the ground planes not being open under the crystal pads?
Thanks Jeff
This may because the Flash doesn't sleep.
You can try to disconnect the power for Flash then test the consumption.
The flash is Winbond W25Q80EWUXIE. Have checked the data sheet power down is B9h
KR