Hi Team,
Iam using DSPS sdk: 6.150.6.77, DA14531MOD.
As per my requirement i have to use DSPS sdk for high data flow.
So, further i want to add other feature like,
1. when BT module not connected to host Application it should be set to command mode.
2. when BT module connected to host Application it should be in data mode.
please let me know at which piece of code App connection and disconnection flags are placed.
Regards,
Laxmi Narayana.
Hi Laxmi,
Thank you for posting your questions online.
This is an good idea, but It is not possible to have both codeless and sps together because the RAM resource are not enough.
You can choose DA1469x and DA1459x for development.
DA14592 - SmartBond Multi-Core Bluetooth® LE 5.2 SoC with Embedded Flash | Renesas
DA14695 - Multi-Core Bluetooth® 5.2 SoC with System Power Management Unit | Renesas
BR,
JH_Renesas