want to add command mode and data mode in DSPS sdk.

Hi Team,

Iam using DSPS sdk: 6.150.6.77, DA14531MOD.

As per my requirement i have to use DSPS sdk for high data flow.

So, further i want to add other feature like,

1. when BT module not connected to host Application it should be set to command mode.

2. when BT module connected to host Application it should be in data mode.

please let me know at which piece of code App connection and disconnection flags are placed.

Regards,

Laxmi Narayana.

Parents Reply Children
No Data