Issue with Debugging DA14531 After Programming OTP

Hi Everyone,

I'm using the DA14531. After I programmed the code into the OTP and set the flags to "YES" for the chip to boot from the OTP, the device can boot from the OTP. However, when I try to debug on Keil, it shows the error "No Cortex-M SW device Found." When I use SmartSnippets Toolbox to connect, it also cannot detect the device. I encounter this issue on both the custom board and the Devkit (Daughter board, mother board). Does anyone have any suggestions regarding this issue?

Thanks.