Hi Sir,
We are using the DA14531 MOD in my design. As per the datasheet P0.0 (J12) is the RESET Pin and Logic high on the P0.0 pin make the module Reset.
We are using a transistor circuit to reset the module, The input of the transistor circuit from microcontroller.
"But the module only working ( Program) when the R304 is removed state"
We cross checked the base voltage of transistor is 0.7V and at the time collector voltage is upto 120mV.
We also check with by changing the R304 resistor values low(4.7K) and high(20K).
Could you please suggest what will be issue? what modifications we needs to make