DA145xx_CODELESS can't show return message by UART

Hi 

I use  CODELESS_6.380.18.63 with EVB DA14531-00.

6.380.18.63\binaries\531-00\

codeless_531_00_datapump.bin & codeless_531_00_set_two_standalone.bin &codeless_531_00_standalone.bin

1.What is the difference between the three of them?
2.If the customized version is paired with DA14530, can I use the firmware of DA14531?
3.The customized version of DA14530 only has 2-wire UART connection and no flash. Which firmware file is recommended?

4.Will the BLE firmware affect whether to use UART or SPI?

Using the APP console(ios) to send AT commands is a normal response.

5.Why does Invalid Input appear when I enter the correct AT command using the codeless_Host application? (input : –>ATI )


The picture below shows the codeless_Host connection settings: