DA14531MOD flash from external MCU through one-wire UART

Hello, i need to flash DA14531MOD from an external MCU via one-wire UART.

I have already tried the example BLE_SDK6_examples/interfaces/external-processor-stm32 at main · dialog-semiconductor/BLE_SDK6_examples (github.com)

but i can this load the fw in RAM and not in FLASH.

I can Flash DA14531MOD from SmartSnippets toolbox (one Wire uart) and i need to do the same thing from my MCU.

I need to tell more info in the Header messagge or set some options?

there are some documents or example that describe this option or how to write the Codeless fw in Flash from external MUC uart?

Thank you in advance.

Andrea